STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L Discovery Blue/Green Led not working

Posted on March 19, 2013 at 02:13Hi, I managed to compile and start the Temperature Measurement Example with Eclipse and Code Sorcery. It runs and shows a temperature. I wanted to add a few lines of code to see the LEDs blinking inside the infinite ...

lawi by Associate
  • 940 Views
  • 1 replies
  • 0 kudos

toggle led with delay inside exti interruption

Posted on March 18, 2013 at 20:53Hi,I am trying to toggle a led inside an EXTI interruption with Delay. The delay function is based on the systick intrruption. Everything works fine seperately but when I try to use the delay inside the EXTI interrup...

DMA for unknown datareceive throw USART

Posted on March 18, 2013 at 15:24Hello, I am working on a device which one funcion should be USART to Ethernet bridge on STM32F407. I need to receive data from USART and then work with them. But beacuse of speed I wanted to use DMA instead of interr...

phajek by Associate
  • 2214 Views
  • 4 replies
  • 0 kudos

STM32F103C6 Increase flash page erase time with IWDG active

Posted on February 28, 2013 at 11:58Hi, I've noticed an extra time in the erase page process when the IWDG is active. I haven't measured it (I notice a change in the blinking frequency of a led) and it's not a big deal, but I can't find any referenc...

xbalmes by Associate II
  • 3615 Views
  • 9 replies
  • 0 kudos

STM32L-DEV (STM32L152RBT6) + I2C with interrupts

Posted on March 17, 2013 at 20:42Hello,I'm new in ST micro controllers. I'm trying to write I2C application that sends and receives data with interrupts, but I can't find information about it.May be anybody knows where to find examples of code of it...

STM32F10x_DSP_Lib_V2.0.0 where to find?

Posted on March 17, 2013 at 20:17Hi All! I just start with stm32 exacly with STM32F103VBT6, i have evaluation kit and i need library named: STM32F10x_DSP_Lib_V2.0.0 and sd_stm32.c where i may find it? Thanks for You patience! #lmgtfy

STM32 USART DR unavailable

Posted on March 14, 2013 at 09:35 Hey, guys! I have one stupid error, show me the right way, please. I'm actually working with STM32L-Discovery and trying firstly to work out the USART. I've done all necessary configurations for th...

dima by Associate II
  • 3584 Views
  • 6 replies
  • 1 kudos

STM32F4 RTC and LSI question

Posted on March 17, 2013 at 15:31Hi I'm just wondering why the LSI on the STM32F4 Discovery board has inaccuracy's, I've searched the internet and application notes but can't seem to find the answer? My seconds on LCD jumps several times between 0-6...

bee2 by Associate II
  • 2000 Views
  • 4 replies
  • 0 kudos

low power mode (snapshot) on OV2640

Posted on March 17, 2013 at 17:37I'm working on a project where power consumption is a critical issue. I need to store a frame from a camera (OV2640) on the uSD each 2 seconds. My problem is that the camera's clock is always on which bring the power...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.