STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

f4-discovery, fpu not working in timer interrupt?

Posted on May 21, 2013 at 16:55Hi, I'm testing the f4 and the fpu. I have a small fpu test like this:volatile float a=0;volatile float b=.1;int c;for(;;)    {      GPIOD->ODR^=0x8000;      for (c=0;c<100;c++)        a=a+b;    }So by looking at PD15 ...

ian239955 by Associate II
  • 1542 Views
  • 3 replies
  • 0 kudos

HardFault_Handler exception...

Posted on May 16, 2013 at 13:53Hello,I'm using the STM32F4 on the discovery evaluation board.I wrote a simple function that calculates the mean of a vector. When the code is starting to make the summation it goes to HardFault_Handler...Here is the m...

0690X00000604sxQAA.png
yoav by Associate II
  • 4650 Views
  • 10 replies
  • 0 kudos

STM32F2xx OTP issue

Posted on April 02, 2013 at 16:47I need to put some data permanent in the OTP. But I phase a few problem durring debbug. 1. When try to program it on power up like in the FLASH I get the error can't program address 0x1FFF7800 as it is not a part of ...

Barbie by Associate II
  • 4639 Views
  • 14 replies
  • 0 kudos

Timer Set up conf: intriguing issue.

Posted on May 20, 2013 at 16:04Hi Folks I have this simple example program that I am modifying and by moving one statement into a while statement it breaks it. I'm working on the STM32F4 Discovery boardHere is the code:- /* =========================...

bl by Associate II
  • 1967 Views
  • 4 replies
  • 0 kudos

measure or integrate an external pulse train

Posted on May 20, 2013 at 18:12I have an external device that I need to measure it's utilization.  I don't need code but I value the discussion and techniques offered.   target is STM32F407The external device outputs a pulse.  minimum pulse width is...

Measuring MIPS of a DSP function using systick

Posted on May 20, 2013 at 15:39Hi all, I have a DSP function and I want to know how many MIPS does it consume. I have used SYSTICK of STM32F2xx device (max frequency 120 MHz) to measure the number of cycles required and now I want  to convert to MIP...

STM32F10x DSP library, where is it?

Posted on May 17, 2013 at 09:48I looking for a download link of the STM32F10x DSP Library, there multiple references to it and a user manual (UM0585) but cannot find the actual code anywhere... Anyone?

ioannis2 by Associate II
  • 1810 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.