STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32f4: How fast can GPIO really be updated?

Posted on June 02, 2013 at 21:41I am using the STM32f4 series. My goal to drive an external parallel loaded DAC using data from the internal SRAM. So, I need to update the data on a GPIO port and then toggle a pin connected to the load control signa...

michael2 by Associate II
  • 2970 Views
  • 4 replies
  • 0 kudos

MCO1 an low power mode

Posted on June 03, 2013 at 15:35Hi,I want to use MCO1 to control an external device using the LSE RTC crystal 32Khz. Does any body know what is the behaviour of MCO1 in stopped or standby mode for STM32F2 device?Thanks. #mco-low-power

Adalgiso by Associate II
  • 834 Views
  • 1 replies
  • 0 kudos

SQRT in stm32f4 ?

Posted on June 03, 2013 at 15:06Hello I want to use sqrt (square root) function to calculate sqrt (x^2 + y^2) but i haven't math.h in my root this is the error  undefined reference to `sqrt'  collect2: ld returned 1 exit status how can i fix it ple...

bmwael1 by Associate II
  • 3298 Views
  • 1 replies
  • 0 kudos

Atollic variables

Posted on June 03, 2013 at 10:42Hello, I'm currently programmed a STM32F4 Discovery with the IDE Atollic. In my program, I get two fonction, the first in the file ''stm32f4xx_it.c'' and the second in the file main.c and i want to known if i can tran...

GPIO pin toggle speed?

Posted on June 03, 2013 at 13:36Anyone know the fastest possible frequency that any GPIO pin state can be toggled?

michael2 by Associate II
  • 1465 Views
  • 2 replies
  • 0 kudos

SPI1 on STM32F4Discovery

Posted on June 02, 2013 at 15:52Hi community, for a few days i try to use the SPI1 on the F4Discovery board. I use the PA5-PA7 pins on AF5. But after my init the code does nothing? What is wrong in my init function? #define Open_SPI_MISO_PIN        ...

dennis23 by Associate II
  • 1476 Views
  • 3 replies
  • 0 kudos

stm32F4discovery usb problem

Posted on June 01, 2013 at 17:05I have implemented the code of this linkhttp://www.st.com/web/en/catalog/tools/FM116/SC959/SS1532/PF252419 that allows sending and receiving a file from a flash drive via the usb stm .. but the problem is that an indi...

STM32F4 Discovery and Rn-41 Bluetooth module

Posted on June 02, 2013 at 23:56Hi, Iam completely new and lost, i want to interface a bluetooth module, I have found some examples but i cannot receive any data on hyperterminal when i run these codes. Actually i need help to find out from where i ...

problem with jtag tck pin

Posted on June 01, 2013 at 08:55hiI have a problem with jtag tck pin on my board.When I touch it with my finger  the st-link Works properly & connect to stm32f417 but if  i remove my finger from this pin the st-link not connect to my mcu.i pull-down...

m2399 by Associate II
  • 1507 Views
  • 2 replies
  • 0 kudos

SD card on STM3240

Posted on May 31, 2013 at 16:15Hello, I need some help with creating fat files on  microSD.I found some files on the demo builder but it only provied viewing directories.Many thanks.

bouhoula by Associate II
  • 2586 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.