2013-05-31 7:15 AM
Hello,
I need some help with creating fat files on microSD.I found some files on the demo builder but it only provied viewing directories.Many thanks.2013-05-31 7:25 AM
FatFs is usually used to access and create files. The access methods are quite similar to STDIO file functions, and documented on the FatFs web page with examples.
I don't have an STM3240(G-EVAL) myself, but have ported SDIO + FatFs to the STM32F4-Discovery, STM324x9I-EVAL, and a host of other custom F2 and F4 boards.2013-05-31 7:33 AM
Thanks for the quick reply, it's not my main job to develop it , I was looking for a ready API.
2013-05-31 7:45 AM
Thanks for the quick reply, it's not my main job to develop it , I was looking for a ready API.
You must be a Java guy. FatFs provides a well documented ''API'', the examples from ST do all the hard integration work.http://elm-chan.org/fsw/ff/en/open.html
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Writing%20on%20USB-Memory&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=97]Add to file example It's also possible to connect the SDCard to USB via an MSC implementation, that way you can plug the board into a PC via USB, and access the SDCard like a normal flash drive from there.2013-05-31 8:47 AM
Nope, I m working on my eval board with C langage.
Ive found the right API but its working with an OS.My project is creating a webserver without an OS.So I wanted to insert my website pages inside the SD Card.Thats why I need it.2013-05-31 9:42 AM
So basically stitching together the STM32F4x7_ETH_LwIP standalone webserver demo, and replacing the existing in memory file handling with the FatFs+SDIO example code.
2013-06-01 1:28 PM
Exactly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.