STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0 Bare Metal I2C

Trying to write a i2c driver for the stm32f0 and having trouble understanding how this works as im use to the stm32f4 i2c could anyone describe what steps i need to take to write a polling i2c driver or point me to an app note that describes ive ben ...

STM32H755XI gets so hot

I checked with the Uploaded File schematic board. I'm using STM32CubeProgrammer. Connect from PC via UART. I confirmed that the UART is connected with STM32CubeProgrammer. ​Software has not been written yet. In that state, the MCU became so hot that...

MPU_schematic.jpg
TDP_0000 by Associate II
  • 5041 Views
  • 10 replies
  • 0 kudos

Voltage control Loop frequency

Hi I am using X-CUBE-DPOWER to set the parameters for my Buck converter operating conditions on a B-G474E-DPOW1 evaluation board. I am trying to understand how the controller is implemented. For the PWM switching frequency, I know that this is done b...

Milan1367_0-1730351388911.png

Resolved! STM32H723 SDRAM clock

Hi all,I was reading through the documentation of the STM32H723 to find out what clock speed I can configure the FMC to run at using an external SDRAM. Looking at older posts and videos there is mentioned 100 MHz, but when I look at the newer/revised...

elso_0-1717262132914.png
elso by Senior
  • 2776 Views
  • 3 replies
  • 0 kudos

Wrong output

This is a problem about the STM32H745XI-Disco control external AD5791 through SPI. When using Debug to detect the serial port output, the result is consistent with the desired result. However, when using a multimeter to measure the output of the AD57...

YZ_C by Associate
  • 1371 Views
  • 0 replies
  • 0 kudos

Resolved! Low voltage for logic high on Nucleo-G431KB

Hello STM community,I have a problem with my Nucleo-G431KB. I am trying to communicate to a sensor device over SPI. The problem I have is that when I use PA5 as SPI1_SCK, the logic high is only 1.4 V instead of the 3.3 V on other pins. When I configu...

EXTERNAL OSCILLATOR

 I AM USING STM32F407G-DISC1 BOARD FOR DEVELOPING CUSTOM BOARD.HERE AN OSCILLATOR IS CONNECTED TO PH1 AND PH2 PINS. IS IT IS COMPALSORY FOR DEVELOPING CUSTOM BOARD?

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.