STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FFT Problem on STM32F4

Posted on April 15, 2013 at 14:53 Hi there, I am writing my Bachelorthesis and have to calculate the FFT on the STM32F4. The Input Signal comes from a Radarsensor and is added with quite a lot of noise. My Radarsensor is powered with a triang...

STM32F2 Enter Bootloader

Posted on July 22, 2013 at 14:37Hi everyone, is it possible to enter the bootmode without setting the Boot0/1-pins with an external switch?

Does TIM10/11/13/14 of STM32F4 support OPM mode?

Posted on July 21, 2013 at 17:39In the register description in the page 516 of STM32F4 reference manual, there are no OPM bit in CR1 of TIM10/11/13/14, but the description says nothing about it doesn't support this feature, and the function TIM_Sele...

STM32F407VGT6 + Kamera (OV7670) + Ethernet Stream

Posted on May 28, 2013 at 18:46Hello, I currently have the problem of the camera (OV7670) via Ethernet (UDP) to stream. I currently use the demo software and a simple UDP connection (server) to build, now I want to send the camera data in JPEG form...

samet by Associate
  • 1977 Views
  • 3 replies
  • 0 kudos

Announcement: Visual Studio support for STM32 devices

Posted on July 09, 2013 at 07:08 Hi, We would like to announce that we have added support for STM32 devices to VisualGDB, our Visual Studio plugin for developing and debugging of embedded projects. A detailed step-by-step guid...

ivan2 by Associate II
  • 1149 Views
  • 1 replies
  • 0 kudos

Keil: Error-Flash-download-failed-Cortex-M0

Posted on July 21, 2013 at 23:58Hi, use the STM32F103 microcontroller for my thesis. The firmware uses different Timer, 2 ADC, SPI and some GPIOs. Until yesterday everything worked perfectly but since I decided to use two timers in master / slave ...

fedex03 by Associate II
  • 2352 Views
  • 1 replies
  • 0 kudos

strange current consumption

Posted on July 21, 2013 at 12:56Hi All, i have issue with current on STM32F417 (100pins) :( when i connect power and BOOT0 is set to run into STM's bootloader i have power consumption 88mA, and when i jump into my program i have 120mA :( i have ...

F2 - unused i/o

Posted on July 20, 2013 at 12:33Hi, I am a little unclear as to what Section 5.6 of AN3320 is recommending for unused I/O pins. For example is configuring a pin as output low, open drain, with internal pull down resistor and unconnected pin, materia...

anthony by Associate
  • 1576 Views
  • 2 replies
  • 0 kudos

Timer 6 and timer 7 on discoveryf407VG

Posted on July 20, 2013 at 11:52Hello every one!I am using MicroXplorer to config timer 6 and timer 7, projrect with devide stm32f407vg. But I can't see it any where!!!When I creat new project, I have timer from timer 1 to 5 and from 8 to 14. But ti...

21003218 by Associate II
  • 1713 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.