2013-07-17 12:35 AM
I have some weird problems with my STM32f4 07 VG board for many days.
First, each debug session launches an error message : no source available for '''' Secondly, there is a problem with address memory, I have such a code in my main program : float32_t var; function(&var);And a function :
void function(float32_t* x){ *x = 1.; }But, oddly, when I debug this code, the x address doesn't fit the var address (x address is 0x00000000 pointer in function) and the value of var is not 1 after function calling. Why do I have this problem ?
In fact, the debugger seems to be broken, during a debugging session, various instructions are omitted... like for loop... I use the GCC GNU ARM compiler (with CooCox IDE) with these options : -mcpu=cortex-m4; -mthumb; -Wall; -ffunction-sections; -g; -O0; -fno-builtin; -DSTM32F407VG; -DSTM32F4XX; -I.; Sorry for my english...Thks. #stm32 #discovery #pinning-tail-on-donkey #free-the-mallocs2013-07-17 4:36 AM
Sounds like problems on the CooCox end, suggest you discuss with them, on their forum.
2013-07-18 1:57 AM
Hi,
I check with a flag variable in STMStudio and the problem really comes from the micro controller.If I create a vector of a size too large, for example 256 float32_t, the loop to fill this vector is omitted and I have a HardFault Interruption...Error accessing memory address 0x0Indeed in my functions, all variables address are set to 0x0 and all my variables are to 0. So, there is a memory problem.I don't understand theses memory problems because I don't overflow the memory ????Thks for your help !
2013-07-18 4:49 AM
the problem really comes from the micro controller...So, there is a memory problem.
The micro just does what you instruct it to do, I'm not convinced that the problem isn't with the tools (compiler/linker). What does the .MAP or .LST file indicate about the created code? Does the tool chain come with any working example projects you can test independently of your own code? Perhaps there is a problem with how your project is set up, or the start up code? There is very little support here of CooCox, as mentioned they do have a forum of their own. Try using Keil or IAR evals For more assistance here you might want to post a complete example of what you're doing. Be aware that exiting main() will likely cause a fault.
2013-07-18 8:09 AM
When I declare my tables with the keyword static I dont't have anymore the HardFault interruption. But the ''No source available for '''' '' is still there...
Can you explain me why the bug seems to disappear by using static variables ?I will try an example yes.Thks.2013-07-18 8:47 AM
why not post your code?
2013-07-18 9:46 AM
Can you explain me why the bug seems to disappear by using static variables ?
Your stack is inadequately sized for the locals/automatics you're attempting to allocate?2013-07-19 12:14 AM
@rocketdaw
Which code, soon as declare a table with a too big size, I have HardFault Exception... The code takes hundred lines, but the initial bug refers to this table... Don't need to post any code.I just want to know how to deal with this problem.@clive1Thanks for help, what do you mean by ''your stack is inadequatly sized...'', I am quite a new in micro controllers field.Thanks.2013-07-19 2:06 AM
Local variables are stored on a stack, if the stack is designed to hold 1024 bytes you can't define an array that takes 8
From startup_stm32f4xx.s in Keil
; Amount of memory (in bytes) allocated for Stack
; Tailor this value to your application needs
; <
h
> Stack Configuration
; <
o
> Stack Size (in Bytes) <
0x0-0xFFFFFFFF:8
>
; </
h
>
Stack_Size EQU 0x00000400
AREA STACK, NOINIT, READWRITE, ALIGN=3
Stack_Mem SPACE Stack_Size
__initial_sp
void test1(void)
{
double array[1024]; // takes 8192 bytes of stack
// do something with array
}
void test2(void)
{
static double array[1024]; // takes 8192 bytes of preallocated RAM
// do something with array
}
2013-07-19 2:47 AM
Ok, good !
So, I just need to redefine this stack size ? Are they counter-argument to redefine it ?Thks.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.