STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F3 Timer3 and Timer4 as PWM

Posted on September 22, 2013 at 22:46Hi,  i use a STM32f3discovery evaluation board and trying to generate 6 PWM signals. For this purpose i have choosen Timers 3 and 4. As base project i use a Demo project. (The project demonstrates a sensors func...

dmytro by Associate
  • 2472 Views
  • 4 replies
  • 0 kudos

Timer to generate SPI clock

Posted on September 22, 2013 at 20:50I am currently reading a high speed ADC over SPI1.  E11 is configured to generate a DMA SPI write/read when the busy signal from the ADC goes low.  A double buffered DMA moves the data from SPI to memory.  Works ...

holcomb by Associate
  • 788 Views
  • 0 replies
  • 0 kudos

F103 not generating spi tx buffer empty interrupt?

Posted on September 20, 2013 at 18:13 I am puzzled over a missing SPI TX buffer empty interrupt at the end of a transmission. In slave mode I transmit x bytes and disable the tx interrupt when a new tx empty interrupt is generated after the ...

bernd by Associate II
  • 1747 Views
  • 2 replies
  • 0 kudos

support for stemwin on stm32f4 discovery

Posted on September 11, 2013 at 08:51Dear sir,            I'm using stm32f4discovery board with DM-STF4BB Base Board and DM-LCD35RT 3.5 inch LCD with touch screen. You can look for details in http://www.embedinfo.com/. Now I need to use your STemWin...

sen by Associate II
  • 1833 Views
  • 4 replies
  • 0 kudos

STM32F4Discovery + STemWIN

Posted on September 16, 2013 at 14:58 Hy guys, I have a problem whit Stm32F4Discovery with 3,5LCD (SSD2119 LCD driver) and STemWIN port. I download the examples from the st website, and try to port to discovery but not working. I have a ...

totti001 by Associate II
  • 1404 Views
  • 4 replies
  • 0 kudos

STM32L152 is not flashable

Posted on September 05, 2013 at 14:42Dear Community, i have an STM32L-Discovery Board with 24 segment display. I wanted to flash a programm with Keil uVision V4.70.0.0 (STLink is set to SW, but no Cortex M device is found), with IAR Embedded Workben...

itfreak12 by Associate II
  • 4057 Views
  • 11 replies
  • 0 kudos

No NAND flash on STM3220G-Eval

Posted on September 13, 2013 at 12:20Hi all,I would like to evaluate the NAND flash interface with the STM3220G-Eval board. However, this board is not populated with the NAND flash, although the board has an estate-area for it. If I were to buy a fl...

tzewan by Associate II
  • 1068 Views
  • 2 replies
  • 0 kudos

ITM data missing

Posted on September 18, 2013 at 21:21Hello. Could some one help to solve a problem with ITM on STM32? I try to use ITM to log data, but some data is missing every time, may be some buffer is overflowing I don't know. I also try different STM32 contr...

cg by Associate II
  • 2359 Views
  • 7 replies
  • 0 kudos

STM32F207ZGT6

Posted on August 18, 2013 at 12:07Dear All, We are using STM32F207ZGT6 in our product which is used for CAN & Ethernet communication.Recently we observed one issue in our board.Board will goto non working condition suddenly and if we connect ST link...

mohana by Associate
  • 997 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.