STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I2C interface through DMA

Posted on September 28, 2013 at 18:03 Hi, I have a long configuration to be done through I2C interface, so I thought I have to do it using DMA.I am trying to read device ID as a start. The problem is that the I2C sequence doesn't reach the...

What's difference between these several register?

Posted on September 15, 2013 at 14:25Hi everybody i have three primary questions. 1- What's difference between GPIOx_CRL rigester and GPIOx_CRH rigester? B.T.W: yeah, i know these both configure the GPIO to input or output modes and speed of output ...

r3 reset when return from ISR

Posted on September 27, 2013 at 17:34I have a really baffling problem.  Perhaps it is not even a problem.  It's just something I noticed when debugging my program.  Register 3 goes to it's reset value when I return from an interrupt service routine....

drobison by Associate II
  • 2312 Views
  • 3 replies
  • 0 kudos

Timers - Port from F4 to F1

Posted on September 02, 2013 at 01:42 The code above is part of a library to control 2 stepper motor for STM32F4. I pretend to use it with STM32F1. 1- Lines 43 to 46 configure the GPIO to Outupo with PushPull, the two lines that I added a...

ee06091 by Associate III
  • 1164 Views
  • 1 replies
  • 0 kudos

using Keil RL-RTX with STemWin

Posted on September 27, 2013 at 09:17 Dear Sir, I'm using STM32F4-DISCOVERY. I've to run the STemWin on this board with keil RL-RTX. I've made all the necessary GUI and LCD configurations and have added GUI_X_RTX.c from the Segger folder in Keil uVi...

sen2 by Associate II
  • 2022 Views
  • 3 replies
  • 0 kudos

Minimizing power consumption: what can be done?

Posted on September 27, 2013 at 16:54HiI'm a bit confused with all the clocks and power saving options on the STM32F3 Discovery board.I'd like to minimize the power consumption by gating all unnecessary clocks and peripherals / memory.The MCU is in ...

WFI problem: Internal command error

Posted on September 27, 2013 at 14:10 Hi I run this very simple code on the STM32F3 Discovery board: int main(void) { __WFI(); return 0; } It compiles fine and I can flash it onto the STM without any problems (I'm using the ST...

STM32 SPI Issue

Posted on August 03, 2011 at 08:24Hai, I am using STM32F103ZE I am not getting SPI data correctly. Master is transmitting correctly. But always read as zero where a non zero value has been sent. Master config: (MSP430) The master configuration is c...

harikk09 by Associate II
  • 5887 Views
  • 11 replies
  • 0 kudos

USART2 problem

Posted on May 02, 2013 at 19:16The original post was too long to process during our migration. Please click on the attachment to read the original post.

yogee00 by Associate II
  • 12212 Views
  • 16 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.