STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with reading ADC channels group using DMA

Posted on September 30, 2013 at 11:35 I am using STM32F407VG. I've read documentation about ADC and groups and still don't know how to set up properly ADC to sample periodically fixed ADC channels. I've done this by following code but don't ...

pawwodko by Associate II
  • 5413 Views
  • 5 replies
  • 0 kudos

EXTI same line different port?

Posted on October 01, 2013 at 09:52Hi, I'm experimenting with interrupts from port pins, I can make the basic example work. What I was trying to do is to create and EXTI interrupt from GPIOA bit 0 and also GPIOB bit 0, but I'm starting to think that...

ian239955 by Associate II
  • 1623 Views
  • 3 replies
  • 0 kudos

From I2C to SPI using the DMA (STM32F0)

Posted on September 25, 2013 at 11:33Hello everybody, I have to communicate with a STM32F0 using the I2C and then, the STM32F0 has to communicate with another device through the SPI? Is it possible to implement it through the DMA? If yyes, do you ha...

STM32F103R4 APB2 interfaces not working

Posted on September 30, 2013 at 21:36Hi My name is Salil and i am a product design engineer with EZ metrology.We are currently using STM32F103R4 in one of our developing products. This product uses only one USART interface (that works) and simple GP...

spuri by Associate
  • 1203 Views
  • 1 replies
  • 0 kudos

OPI Driver ERROR 231

Posted on September 30, 2013 at 13:19hi,I am using STM32RBT6 and RIDE7,when I try to debug there is an error ''unable to reset device and enter to debug mode''can you help me?

aymen by Associate II
  • 1595 Views
  • 3 replies
  • 0 kudos

Fatal Error[Pe1696]

Posted on September 30, 2013 at 13:50The original post was too long to process during our migration. Please click on the attachment to read the original post.

udif26 by Associate
  • 1349 Views
  • 1 replies
  • 0 kudos

ADC reading problem

Posted on September 28, 2013 at 21:19 Hi all This task is absolutely simple and I'm really wondering why i'm having a problem with it. I'm supposed to read the battery level via the ADC on stm32f100c8. What i'm doing is completely ...

sherif by Associate II
  • 1877 Views
  • 3 replies
  • 0 kudos

VCP with STM32

Posted on June 01, 2012 at 15:43Hello, I am working on virtual serial port to communicate between computer and device through usb. So i downloaded ''STM32F105/7,STM32F2 and STM32F4 USB on-the-go Host and device library.''  from http://www.st.com/sto...

hisham23 by Associate III
  • 6551 Views
  • 12 replies
  • 0 kudos

SPI fastest receive method

Posted on September 27, 2013 at 11:21Hello, I'm trying to receive data on an STM32F205 SPI1 as fast as possible. The sender is a STM32F4, and it sends commands in different lengths up to 2048 Bytes per command. There is no OS on the receiver, just t...

mail2 by Associate II
  • 2271 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.