STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Understanding the purpose of ADC_SMPR

Posted on October 13, 2013 at 06:46Hi,I'm trying to understand what the ADC_SMPR register is used for.According to Reference Manual we have following control on the ADC conversion time:ADC_CR1 Register:Bits 25:24 RES[1:0]: ResolutionThese bits are w...

dimax by Senior
  • 2635 Views
  • 5 replies
  • 0 kudos

STM32F3 - ARM Cortex-M4 32-Bit MCU- SPI

Posted on October 07, 2013 at 21:54Hi, I am using the Discovery F3, I am trying to interface with an SPI port device which requires a 32 bit transfer and 8 bits for address, in the data sheet, the data size is between 4 and 16 bits. I would know if ...

SPI BSY flag

Posted on February 22, 2012 at 17:14Dear All, I have two separate STM32F103's communicating to each other by SPI. I've configured one as a master & the other as a slave. I'm using DMA to automate the SPI transfer. I've used the ST Library (3.5.0) e...

delay func using TIM2

Posted on October 12, 2013 at 18:10 I want to write function using timer 2 for have millisecond in STM32F103 I just don't know why this doesn't work! TIMER2 config: void config_TIM2() { NVIC_InitTypeDef NVIC_InitStructur...

_behn4m by Associate II
  • 1160 Views
  • 1 replies
  • 0 kudos

PA11 and PA12 on STM32F3 discovery

Posted on October 11, 2013 at 20:44 hi, below is the code i wrote just to change the states of pins PA10, PA11, PA12 and PA even though pin PA10 and pin PA15 gives the correct output to the functionsGPIO_SetBits() andGPIO_ResetBits(); PA11...

hendalage by Associate II
  • 1585 Views
  • 1 replies
  • 0 kudos

rename ''STMicroelectronics Virtual COM Port''

Posted on October 11, 2013 at 09:54Hi, I have USB virtual com port working fine, with the demo code, it appears as ''STMicroelectronics Virtual COM Port'' in the Windows device manager.Is there some way I can modify the text so I can make it show <m...

ian239955 by Associate II
  • 1051 Views
  • 1 replies
  • 0 kudos

SWD Hardware question

Posted on October 10, 2013 at 05:18Hi, I am new to the STM32 MCU.I am confused as to how to do In-circuit Serial programming with STM32F0 processors.F0 line doesn't seem to have JTAG option, but it has SWD option.So, For SWD, how should the DATA,CLK...

Use of multiple analog functions of same pin possible?

Posted on September 10, 2013 at 15:32Hello guys! I wonder if it is possible to use more than one additional function if the pin is configured as an analog input. I can not find any detail in the datasheet or reference manual that denies or allows th...

STM32F205 TIM5 PWM frequency calculation?

Posted on October 10, 2013 at 08:20 Hi, I will output a PWM Signal on a STM21F205 Pin A3 and use the following code: GPIO_InitTypeDef GPIO_InitStructure; TIM_TimeBaseInitTypeDef TIM_TimeBaseInitStruct; TIM_OCInitTypeDef TIM_OC...

mail2 by Associate II
  • 1956 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.