STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TIMER in cascade mode example request

Posted on October 25, 2013 at 10:06Hi to everybody, I'm new to STM32F303, my ploblem is I'm not able to found a valid example on where is showen how to configure two timers in the way to use the first one to acquire an encoder's pulses and the secon...

UART1 TX pin as 5V Tolerant - Should be OK?

Posted on October 25, 2013 at 05:54 I'm trying to setup some communications between an STM32L152 series MCU with an ATMEGA The Atmega uses 5V logic high. I read the Datasheet and found that the UART1 RX pin is 5V tolerant on the STM32 so I shoul...

byrned by Associate II
  • 864 Views
  • 0 replies
  • 0 kudos

ADC Clock config

Posted on October 24, 2013 at 16:13Hi there,Lately I'm experimenting with the STM32FXXX. Now I came across a problem when I want to configurate the ADC clock. I want to use the maximum frequency that is possible for the ADC. The manual says that the...

Birdo by Associate II
  • 1390 Views
  • 2 replies
  • 0 kudos

Is KEIL better or IAR for STM32 ?

Posted on October 21, 2013 at 16:37Hi Friends...Is KEIL better or IAR for STM32 ? Code optimization, speed compiling, Debugging !!! What do you think about this ?

New STM32 Project in IAR EWARM

Posted on October 24, 2013 at 19:28How the ''CMSIS'' and ''EWARM '' fields seen in ''workSpace window '' are added in a New IAR EWARM Project , what settings are used while creating project , any Example from ST for stm32xxx comes with a project whi...

akp25i by Associate II
  • 1130 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.