2013-10-24 10:28 AM
How the ''CMSIS'' and ''EWARM '' fields seen in ''workSpace window '' are added in a New IAR EWARM Project , what settings are used while creating project , any Example from ST for stm32xxx comes with a project which has These fields , but when i create a new IAR project for stm32xxxx , these fields are not added by default , i select ''Use CMSIS'' in Project->option->General option->Library configuration , but still ''CMSIS'' component does not appears in , neither ''EWARM'' component , are these Fields added Manually , since they are part of almost every ST cortexm3 example i think they should be generated by IAR
#know-your-tools2013-10-24 12:27 PM
i think they should be generated by IAR
Perhaps, but I think that is something IAR expects the developer to manage. ST provides TEMPLATE projects for the explicit purpose of providing a starting point without going into the minutia of creating a project and all the attendant meta-data related to include paths, and defines. The developer is expect to be able to drive the tools they purchased. I'd strongly suggest you navigate your way around the template project, and understand how it is constructed, and what settings/options are desirable for your application.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.