2013-12-05 8:35 PM
Our team is applying MCU STM32F207 to 800x480 touch LCD. We have connected external flash memories both NAND and NOR to our board for huge image data. We want to use MCU RAM for program codes and external memories for the image data.
Can we get the information about how to compile with IAR EWARM compiler for this?
Thanks and Regards
Shin-Young Kwon
</p>
</span>
#external-memory2013-12-06 12:59 AM
for
information
on how to configure
the .icf file you can read the template included in ST standard library package (I have the STM32F4 library I don't know the STM32F2 serie but I think you can found the template also for this micro) The readme file included in template directory say:- project .ewd/.eww/.ewp: A pre-configured project file with the provided library
structure that produces an executable image with IAR
Embedded Workbench.
- stm32f4xx_flash.icf : This file is the IAR Linker configuration file used to
place program code (readonly) in internal FLASH and data
(readwrite, Stack and Heap)in internal SRAM.
You can customize this file to your need.
- stm32f4xx_flash_extsram.icf: This file is the IAR Linker configuration file
used to place program code (readonly) in internal
FLASH and data (readwrite, Stack and Heap)in
external SRAM. You can customize this file to your need.
- stm32f4xx_flash_extsdram.icf: This file is the IAR Linker configuration file
used to place program code (readonly) in internal
FLASH and data (readwrite, Stack and Heap)in
external SDRAM. You can customize this file to your need.
- stm32f4xx_ram.icf: This file is the IAR Linker configuration file used to
place program code (readonly) and data (readwrite, Stack
and Heap)in internal SRAM.
You can customize this file to your need.
2013-12-08 4:26 PM
Thank you so much for your help. We will try to find that template!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.