STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interrupt priority problem

Posted on January 08, 2014 at 16:06HiI'm working on a project where I use a interrupt from the RTC. This is the one second interrupt. I also use a couple of other interrupts, for example timer 3. The RTC interrup can have the lowest interrupt possib...

m_ by Associate II
  • 3696 Views
  • 8 replies
  • 0 kudos

EXTI line 13 always pending? (STM32F103VG) Solved!

Posted on January 10, 2014 at 06:05Hello all, hopefully someone can see the error of my ways? I have a some hardware with a couple of rf modules IO lines connected to Port D pins 10, 11, 12, 13. All is well except for pin 13 which is always providin...

Help me choose a programmer [newbie]

Posted on January 08, 2014 at 21:05I have a legacy system that uses a STM32F103RE device and I would like to connect to it via JTAG (or any other on board option) and view the code on the device to verify it's version (and possibly update).  It seem...

STM32f-Discovery USART send BREAK

Posted on January 09, 2014 at 17:19I have setup the USART to Tx/Rx however my application requires sending a Break. The STM32F programmer's manual refernces sending Idle and Break, provides an example and register for sending an idle character but n...

vendor by Associate II
  • 2362 Views
  • 4 replies
  • 0 kudos

STM32F103 USB Virtual COM problem

Posted on October 25, 2013 at 16:13Hi, I am using olimex kit of  STM32F103RBT6 microcontroller. I am new in USB virtual COM programming. I am using STM32_USB-FS-Device_Lib_V3.3.0 with Keil MDK-ARM 5.0 IDE. I opened the precompiled Virtual Com port p...

Measuring Vdd through Vbat

Posted on January 07, 2014 at 23:00Using an STM32F407xx, I want to monitor Vdd by connecting it to Vbat and using ADC1_IN18. If I am not actually powering my device from the battery, is it still possible (or advisable) to do this?The reason that I a...

dibs by Associate II
  • 4299 Views
  • 7 replies
  • 0 kudos

Hard Fault test error?

Posted on January 09, 2014 at 13:14In order to test the Hard Fault interrupt, I modified the Systick example on ''STM32F0xx_Discovery_FW_V1.0.0'' as follows.. on main.c I added two lines: ------------------------------ int main(void) { uint8_t* Byte...

How to calculate date,month and year ?

Posted on January 08, 2014 at 08:35Guys, How to calculate date,month and year ? from RTC_GetCounter function, I saw : uint32_t RTC_GetCounter(void) {   uint16_t tmp = 0;   tmp = RTC->CNTL;   return (((uint32_t)RTC->CNTH << 16 ) | tmp) ; } I've done ...

STM32L1xx performance question

Posted on January 04, 2014 at 13:57 Dear Sir/Madam, In the past I have been using 8-bit AVR (Atmega328p) for my application. The application uses the following peripherals: - I2C peripheral and - USART peripheral The ...

klemen by Associate II
  • 3585 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.