STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

(sd)Disk explore

Posted on February 25, 2014 at 18:16Hi,  I am trying to modify function static uint8_t Explore_Disk (char* path , uint8_t recu_level); from USB host example for writing our more than 1 subdirectory and for SD card. I added :             else if(recu...

jspika by Associate II
  • 1180 Views
  • 2 replies
  • 0 kudos

Dma1 Stream6 Uart 2 tx Fifo error

Posted on February 25, 2014 at 04:02 I use the dma to TX only, the rx is handled in a interrupt with no dma. I've been working on this for quite some time now and I Always get a FEIF6 interrupt. Specifically I get TC, HT and FE. I dont h...

STM32F051 KEIL RTX CMSIS Interrupt Handling

Posted on February 25, 2014 at 16:48Hi All, I am new on this forum and as well new to STM32 microcontrollers - almost two months working with them - so please be understanding if I will write something stupid or ask about something obvious. Thanks. ...

damian by Associate II
  • 1361 Views
  • 2 replies
  • 0 kudos

Help with STM32F4 Clock config

Posted on February 25, 2014 at 15:30 Hi guys, I need help to configure the stm32f4 clock to disable the pll and just work with the 8MHz external crystal of the discovery board. The goal is to reduce as much as possible the consumpt...

STM32f-4 Motor control - PWM not generate

Posted on January 16, 2013 at 11:39Hi, i'm using the stm3240f board with a stm32f4-series.I try to generate PWM but nothing happen.what i did : /*declaration-----------------------------------------*/TIM_TimeBaseInitTypeDef  TIM_TimeBaseStructure;TI...

STM32F40/ DSP PERFORMANCE

Posted on February 25, 2014 at 12:11Hi ;   We produce madical instruments ; our main products depends on stm32f407 and we are happy with it ; Now are designing a new product that needs many DSP filters ( FIR + IIR ) ; the sampling rate would be abou...

stm32 timer IC counter reset

Posted on February 25, 2014 at 13:54UPDATE: The TIM_SelectInputTrigger function and the TIM_ITRxExternalClockConfig function both write to the TS bits in the TIMx_SMCR register so the final value is ITR2 overwriting the TI1FP1 value set.  Because I ...

adam by Associate
  • 991 Views
  • 0 replies
  • 0 kudos

stm32f4 and PSRAM

Posted on April 27, 2013 at 17:53The original post was too long to process during our migration. Please click on the attachment to read the original post.

warcatz by Associate II
  • 2484 Views
  • 3 replies
  • 0 kudos

ST-Link (SWD)// STM32F4Discovery

Posted on February 22, 2014 at 14:31I used the discovery kit to prototype a control-board. The self developed board using the stm32F4 MPU works well. Thus far i flashed it with the st link debugger that is integrated into the kit, which worked fine....

fhorvat by Associate
  • 1325 Views
  • 2 replies
  • 0 kudos

System Tick Problem

Posted on February 24, 2014 at 06:27 Hi , I am using STM32F429 discovery. The system tick is suppose to produce an interrupt every 1ms. However, i have gotten 3.12ms instead. Did i make a mistake ? int main(void) { Init_...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.