2013-01-16 2:39 AM
Hi, i'm using the stm3240f board with a stm32f4-series.
I try to generate PWM but nothing happen.what i did : /*declaration-----------------------------------------*/TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;TIM_OCInitTypeDef TIM_OCInitStructure;uint16_t CCR1_Val = 333;uint16_t CCR2_Val = 249;uint16_t CCR3_Val = 166;uint16_t CCR4_Val = 83;uint16_t PrescalerValue = 0;/* Private function prototypes -----------------------------------------------*/void TIM_Config(void);/*MAIN---------------------------------------------------*/int main(void){ TIM_Config(); /* Compute the prescaler value */ PrescalerValue = (uint16_t) ((SystemCoreClock /2) / 21000000) - 1; //slowndown count /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = 665; TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure); /* PWM1 Mode configuration: Channel1 */ TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = CCR1_Val; TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM3, &TIM_OCInitStructure); TIM_OC1PreloadConfig(TIM3, TIM_OCPreload_Enable); /* PWM1 Mode configuration: Channel2 */ TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = CCR2_Val; TIM_OC2Init(TIM3, &TIM_OCInitStructure); TIM_OC2PreloadConfig(TIM3, TIM_OCPreload_Enable); /* PWM1 Mode configuration: Channel3 */ TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = CCR3_Val; TIM_OC3Init(TIM3, &TIM_OCInitStructure); TIM_OC3PreloadConfig(TIM3, TIM_OCPreload_Enable); /* PWM1 Mode configuration: Channel4 */ TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = CCR4_Val; TIM_OC4Init(TIM3, &TIM_OCInitStructure); TIM_OC4PreloadConfig(TIM3, TIM_OCPreload_Enable); TIM_ARRPreloadConfig(TIM3, ENABLE); /* TIM3 enable counter */ TIM_Cmd(TIM3, ENABLE); while (1){ }}/** * @brief Configure the TIM3 Ouput Channels. * @param None * @retval None */void TIM_Config(void){ GPIO_InitTypeDef GPIO_InitStructure; /* TIM3 clock enable */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE); /* GPIOC clock enable */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); /* GPIOC Configuration: TIM3 CH1 (PC6), TIM3 CH2 (PC7), TIM3 CH3 (PC8) and TIM3 CH4 (PC9) */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ; GPIO_Init(GPIOC, &GPIO_InitStructure); /* Connect TIM3 pins to AF2 */ GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_TIM3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_TIM3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource8, GPIO_AF_TIM3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource9, GPIO_AF_TIM3); }I see nothing on the motor control connactor (CN5) exept the 5V on the pin number 25.Any suggestions?Thanks for helping!!2013-01-16 7:27 AM
Well the code doesn't appear unreasonable. You should be able to see a 31.5KHz signal at PC6..9 on the scope. I'd start verifying that and then move further out the circuit, referring to the schematic.
Is there perhaps a control signal enabling the 5V interface, the STM32F4 doesn't output such voltages, look at the buffering circuits? So which board is this exactly? Can you provide a link? STM3240F google-whacks to your singular post.2014-02-25 6:34 AM
Hi clive, sorry but i didnt see ure answer!!
Thank you a lot, but i fixed the problem! That's why i didnt come back on st community^^ My first message i had post, i got no reponse, so thanks for urs!2014-02-25 6:34 AM
Hi clive, sorry but i didnt see ure answer!!
Thank you a lot, but i fixed the problem! That's why i didnt come back on st community^^ My first message i had post, i got no reponse, so thanks for urs!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.