STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DMA does not go to the interrupt handler

Posted on March 07, 2014 at 23:41I got my DMA working fine , and I can perform transfers successfully , but when i enabled the DMA Transfer complete interrupt , it does not go to the handler , ....... the transfer is done successfully and i can see ...

Newbie on stm32 (USB HID or CDC on f3 discovery)

Posted on February 28, 2014 at 23:00Hi, i'm newbie on stm32 and i have some questions about it ! I have f3discovery and i would like to communicate with my pc by usb ! I want to send to my pc the angles values of the gyroscope. On my pc i use Qt. I ...

idealsim by Associate II
  • 921 Views
  • 2 replies
  • 0 kudos

flashing STM32 - BIN specification

Posted on March 07, 2014 at 18:23Hi. I'm writing a pc tool for flashing STM32F407 using USART. I got familiar with AN2606 (bootloader) and AN3155 (USART protocol). One thing I don't know is the BIN file specification. Can I just write to STM32 the c...

blul by Associate II
  • 5464 Views
  • 7 replies
  • 0 kudos

3 channels on ADC1 and DMA

Posted on April 10, 2013 at 07:59 Hi Everbody, I'm trying to configure 3 channels of the ADC (Vbat, Temp and another analog input). Yesterday, I managed to read the value of Vbat. Now I would to read the value of the three channels, but I...

STM32F103 USB communication

Posted on March 07, 2014 at 17:27Hi Hi, I have done some test using the USART1 PA9 and PA10 pin to communicate with my arduino board, i made some basic configuration like this : USART_InitTypeDef USART1_Init;RCC_APB2PeriphClockCmd(RCC_APB2Periph_USA...

jean2 by Associate II
  • 1338 Views
  • 1 replies
  • 0 kudos

CAN Filter configuration

Posted on March 05, 2014 at 13:17Hello guys,Can anyone explain me how CAN filters work? I cannot understand the reference manual, I don�t know if I am stupid or it is very bad explained (stm32f407).I read a lot of post on the internet but I have a m...

The solution for a 800×480 LCD based on STM32

Posted on March 07, 2014 at 10:40Hi everyone,    I'd like to choise STM32 for a HMI case, whoes main requirement was a TFT LCD of 800*480. There were 2 idea: 1) STM32F1 + RA7785 2) STM32F429 Which was the better? Everybody could give me some suggest...

albhuang by Associate II
  • 780 Views
  • 1 replies
  • 0 kudos

Stm32 LIN driver

Posted on November 07, 2013 at 16:50 Hello everybody. I need to use LIN communication with stm32 mikrocontroller. I see the std lib have function for lin communication, but the comments in the usart.c file is strange. The lin communi...

totti001 by Associate II
  • 1308 Views
  • 1 replies
  • 0 kudos

STM32F401 USB without HSE

Posted on March 05, 2014 at 12:59I'm looking at making a device with the STM32F401, and I'm wondering if USB on it can function without a HSE crystal?The clock diagrams seem to imply that PLL48 can work off of HSI, but the reference implies that USB...

gw by Associate II
  • 2748 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.