STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Trigger DMA From CCR Timer

Posted on March 09, 2014 at 20:46Greetings all, I'm new here so I hope I'm doing this right.STM32F0I'm trying to trigger a DMA transfer from TIM2 with CCR1Here's my code for the timer portionTIM_TimeBaseInitTypeDef timerInitStructure;timerInitStruct...

jasonshaw by Associate II
  • 5211 Views
  • 10 replies
  • 0 kudos

Spirit1 Comunication Problem

Posted on March 10, 2014 at 11:29Greetings everybody. I'm here to ask you some advice regarding an issue that's troubling me. I'm working with an STM32F103 microcontroller, connected with a Spirit1 radio. What I'm trying to accomplish is a comunicat...

jacopo by Associate II
  • 2958 Views
  • 8 replies
  • 0 kudos

STM32f4 Discovery- standart peripherial labrary

Posted on March 09, 2014 at 20:43Hi,I have downloaded the STM32F4xx_DSP_StdPeriph_Lib_V1.3.0which contains the standart peripherial labrary and examples:Im trying to study  GPIO & TIM using this examples....I understand the code and the architecture...

titkin by Associate
  • 2614 Views
  • 4 replies
  • 0 kudos

STM32F407 PWM output high on startup

Posted on March 10, 2014 at 02:52 Hi, I'm using the PWM (driven by the DMA controller) to run a line of LEDs. These devices interpret a long high pulse as a start of packet. A pull-down resistor keeps the output in a 'safe' state until the I...

philpem by Associate II
  • 2471 Views
  • 2 replies
  • 0 kudos

STM32F107 USB-OTG documentation

Posted on March 11, 2013 at 22:01Hello everyone,I’m working with STM32F107 and need to use USB-OTG in project. For some reasons OTG library (USB HID throughput) is not good enough. And it seems like OTG_FS programming model chapter in STM32F1x Ref...

ageeav by Associate
  • 2151 Views
  • 4 replies
  • 0 kudos

STM32SnippetsF0

Posted on March 06, 2014 at 15:40A bunch of examples avoiding the ''library''. https://my.st.com/st-extranet-web-active/active/en/news/n3525 http://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1743/PF260157 Way to go, ST. I hope we will see ...

How to debug code freeze in STM32F401

Posted on March 05, 2014 at 01:28Hi, I am running my own code on STM32F401 Discovery board. Sometimes (pretty rarely) the code freezes. I added sufficient logging to HardFault_Handler, but it is not executed. I am not sure, but most likely the code ...

jhnlmn by Associate III
  • 4042 Views
  • 5 replies
  • 0 kudos

SPI and SDcard ?

Posted on March 09, 2014 at 12:38Hello Guys, Is it possible for me using SPI on STM32F103 for SDCard interfacing ? Any library I can use as a reference ? Thank you

FS usb on STM32F3

Posted on March 07, 2014 at 12:10Hi, I have implemented an CDC class on STM32F3 discovery board with the USB-FS library and it works fine. I'm processing data all the time in a while loop that has a frequency of about 50 Khz.After processing i send ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.