STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 USART1 DMA -> clear DMA content

Posted on July 10, 2014 at 11:19Hi I configured the USART1 with the DMA Controller to receive 16 Bytes. In case if I receive just 1 Byte (Error on the line for example or when starting the sytem) then I like to delete the whole content of the DMA Co...

dominik by Senior
  • 2010 Views
  • 3 replies
  • 0 kudos

IAR EWARM zero-length array problem.

Posted on July 10, 2014 at 11:53Sorry for asking a bit of non relevant question here. I feel some experts here can help me out.I was implementing some code from OpenPilot firmware in IAR EWARM, got into a problem.I have described the problem at http...

harinath by Associate III
  • 768 Views
  • 0 replies
  • 0 kudos

STM32F4 SPI buffer overrun problem

Posted on July 10, 2014 at 07:10 Hi, I'm trying to establish SPI communication between PIC18F2580 as master and STM32F4 Discovery as slave. Using logic analyzer,I found that PIC and STM32F4 actually sending bytes (PIC's MOSI and STM3...

flukeco by Associate II
  • 773 Views
  • 0 replies
  • 0 kudos

Microxplorer suggestions for improvement

Posted on October 02, 2013 at 10:05Maybe it'sread bydevelopers from ST. I had two ideas for improvements - Somehow graphically distinguish outputs that are 5 volt tolerant - Add user defined (label) tag in which the user can observe what signal is ...

asrock70 by Associate II
  • 1994 Views
  • 4 replies
  • 0 kudos

STMCubeMX V 4.3.0 STM32F37x

Posted on July 08, 2014 at 19:01Will not allow configuring both USB and CAN at the same time (forces both to PA11/PA12). Trying to configure USB on PA11/PA12 and CAN on PB8/PB9. CAN shows up in override list for PB8/PB9 but pins turn orange and stat...

STM32F4 SPI3 interrupt problem

Posted on July 08, 2014 at 08:25Hello;I am working on stm discovery. My aim is get output from speaker. I did it in main function. but i want to use SPI3 interrupt for send data. My codes in below. The code does not go to interrupt. I put breakpoint...

How do I get the Systick values from register in real-time ?

Posted on July 09, 2014 at 07:51For now, I need to do a simple benchmark of memcpy. Here, it's pseudocode.#define SYSTICKS_REG 0xE000E018uint32_t *get_systicks (void){    return (uint32_t *) SYSTICKS_REG;}measure_start = *get_systicks ();for (int j ...

gapryun by Associate II
  • 2090 Views
  • 2 replies
  • 0 kudos

DMA2 ISR and TIMER ISR conflict

Posted on June 13, 2014 at 20:42Hello,I am confused by a DMA2 ISR and TIMER ISR conflict which is occurring in my project.The project is based upon the FATFS SDIO example project provided with the STM32F4Discovery PCB.I have had no trouble whatsoeve...

forrest by Associate II
  • 2122 Views
  • 6 replies
  • 0 kudos

STM32F407VGT6 System Tick Configuration Issue

Posted on May 27, 2014 at 09:14Hi, I am facing an issue to configure system tick for STM32F407VGT6 discovery board. if (SysTick_Config(SystemCoreClock / 1000) is given in example to configure system tick for 1 milli sec. This board runs with 168MHZ....

STM32F303 USART bootloader: NACK for ''Go'' command?

Posted on July 07, 2014 at 16:20Hi!How can I tell the STM32F303 bootloader to run application code from flash memory? After reading AN3155, I tried the following byte sequence (''>'' indicating bytes sent to the serial interface, ''<'' bytes receive...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.