2014-07-07 11:25 PM
Hello;
I am working on stm discovery. My aim is get output from speaker. I did it in main function. but i want to use SPI3 interrupt for send data. My codes in below. The code does not go to interrupt. I put breakpoint but its not work. I couldnt find my fault. Could anybody help me?Thanks for your answers. This is my codec init, its work fine when i send data to codec in main.void codec_init(){ GPIO_InitTypeDef PinInitStruct; GPIO_StructInit(&PinInitStruct); PinInitStruct.GPIO_Pin = CODEC_RESET_PIN; PinInitStruct.GPIO_Mode = GPIO_Mode_OUT; PinInitStruct.GPIO_PuPd = GPIO_PuPd_DOWN; PinInitStruct.GPIO_OType = GPIO_OType_PP; PinInitStruct.GPIO_Speed = GPIO_Speed_50MHz; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOD | RCC_AHB1Periph_GPIOB, ENABLE); GPIO_Init(GPIOD, &PinInitStruct); PinInitStruct.GPIO_Mode = GPIO_Mode_AF; PinInitStruct.GPIO_OType = GPIO_OType_OD; PinInitStruct.GPIO_Pin = I2C_SCL_PIN | I2C_SDA_PIN; PinInitStruct.GPIO_PuPd = GPIO_PuPd_NOPULL; PinInitStruct.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &PinInitStruct); GPIO_PinAFConfig(GPIOB, GPIO_PinSource6, GPIO_AF_I2C1); GPIO_PinAFConfig(GPIOB, GPIO_PinSource9, GPIO_AF_I2C1); RCC_APB1PeriphClockCmd(RCC_APB1Periph_I2C1 | RCC_APB1Periph_SPI3, ENABLE); RCC_PLLI2SCmd(ENABLE); PinInitStruct.GPIO_OType = GPIO_OType_PP; PinInitStruct.GPIO_Pin = I2S3_SCLK_PIN | I2S3_SD_PIN | I2S3_MCLK_PIN; GPIO_Init(GPIOC, &PinInitStruct); PinInitStruct.GPIO_Pin = I2S3_WS_PIN; GPIO_Init(GPIOA, &PinInitStruct); GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_SPI3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_SPI3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_SPI3); GPIO_PinAFConfig(GPIOC, GPIO_PinSource12, GPIO_AF_SPI3); //keep Codec off for now GPIO_ResetBits(GPIOD, CODEC_RESET_PIN); NVIC_PriorityGroupConfig(NVIC_PriorityGroup_3); NVIC_InitStructure2.NVIC_IRQChannel = SPI3_IRQn; NVIC_InitStructure2.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure2.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure2.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure2); // configure I2S port SPI_I2S_DeInit(CODEC_I2S); I2S_InitType.I2S_AudioFreq = I2S_AudioFreq_16k; I2S_InitType.I2S_MCLKOutput = I2S_MCLKOutput_Enable; I2S_InitType.I2S_DataFormat = I2S_DataFormat_16b; I2S_InitType.I2S_Mode = I2S_Mode_MasterTx; I2S_InitType.I2S_Standard = I2S_Standard_Phillips; I2S_InitType.I2S_CPOL = I2S_CPOL_Low; I2S_Init(CODEC_I2S, &I2S_InitType); I2S_FullDuplexConfig(I2S3ext, &I2S_InitType); // configure I2C port I2C_DeInit(CODEC_I2C); I2C_InitType.I2C_ClockSpeed = 100000; I2C_InitType.I2C_Mode = I2C_Mode_I2C; I2C_InitType.I2C_OwnAddress1 = CORE_I2C_ADDRESS; I2C_InitType.I2C_Ack = I2C_Ack_Enable; I2C_InitType.I2C_AcknowledgedAddress = I2C_AcknowledgedAddress_7bit; I2C_InitType.I2C_DutyCycle = I2C_DutyCycle_2; I2C_Cmd(CODEC_I2C, ENABLE); I2C_Init(CODEC_I2C, &I2C_InitType); SPI_I2S_ITConfig(SPI3, SPI_I2S_IT_TXE, ENABLE);}void I2S3_IRQHANDLER(void) {if(SPI_GetITStatus(SPI3, SPI_I2S_IT_TXE) != RESET){SPI_I2S_SendData(SPI3,Buffer[counter]);} }2014-07-09 1:11 PM
void I2S3_IRQHANDLER(void) {
Case sensitive, use SPI3_IRQHandler ? Or perhaps you have some #define you haven't shared? If you use C++ make sure it's not mangling the name, review .MAP fileWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.