STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F303 - USART.RXNE behaviour when using RX DMA

Posted on July 15, 2014 at 17:21Hi,I am currently implementing a USART rx driver on an STM32F303xxx using a receive DMA buffer. The motivation to use DMA is to allow reception of bursty high speed (8Mbps) data. [note that using HW flow control doesn...

raul by Associate
  • 1133 Views
  • 1 replies
  • 0 kudos

Using the calloc function on an STM32F4

Posted on July 15, 2014 at 17:12I'm trying to understand how this function should be used on an F405 chip. The code that calls calloc is all generated from a simulink fuzzy controller model so I'm confident it's correct in terms of code.The program ...

rajpaged by Associate II
  • 2112 Views
  • 3 replies
  • 0 kudos

usart1 and usart2 contention

Posted on July 15, 2014 at 17:19Hello again. I've two usarts in use on my board. One, Usart1 is connected to the console and the other usart2 is connected to a modem chip. When I enable the usart2 interrupt using the NVIC commands, there is no outpu...

dvcosta43 by Associate II
  • 1849 Views
  • 3 replies
  • 0 kudos

How to convert the systick to ns ?

Posted on July 15, 2014 at 16:18DearI have read Ch14.1 Systicks the definition guide of Cortex M3 2nd. But I still confuse it. If I take the Systicks Reload = 65536, the corresponding time is 65536 * 168 MHz * 1e9 ?Am I correct?  Thanks 

gapryun by Associate II
  • 2952 Views
  • 3 replies
  • 0 kudos

How to convert the DWT CYCCNT to ns ?

Posted on July 15, 2014 at 17:26DearI have read Ch16.2 Trace component DWT, the definition guide of Cortex M3 2nd. But I still confuse it. If I take the CYCCNT, the corresponding time is CYCCNT * 168 MHz * 1e9 ?Am I correct?  Thanks 

gapryun by Associate II
  • 2139 Views
  • 3 replies
  • 0 kudos

STM32 compiled code addresses at 0x0 not 0x08000000

Posted on July 15, 2014 at 14:57Hi all,I saw that the current practice is to compile all code at 0x08000000 offset. This is fine for me, but now I have an application with a lot of constant tables in flash, and more important, a ''host'' application...

raimond by Associate III
  • 2560 Views
  • 3 replies
  • 0 kudos

GDB became very slow in CoIde

Posted on July 15, 2014 at 12:03 Hi everyone, I'm working on a STM32F427 with CoIde on Windows Vista for a long time now without any issue. Since yesterday my debugger became very slow, very very slow. when i hit the ''pause'' button it takes approx...

benoit2 by Associate II
  • 1749 Views
  • 3 replies
  • 0 kudos

DMA2 problems: NDTR not zero

Posted on July 09, 2014 at 18:40I'm having some problems with DMA transfers apparently stalling on our STM32F405ZGT6 board. The problem seems to only happen when I have multiple streams running. So, I have Stream3 using SDIO, with 32 bit wide access...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.