STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Integrated Debugging in Eclipse

Posted on July 16, 2014 at 16:03Hi, I recently buy a STM32L152 Nucleo, I begin with mbed.org but I prefer to develop offline. So I was wondering if there are any plug-ins to debug my programs. I follow this tutorial : http://erika.tuxfamily.org/wi...

alain by Associate II
  • 2499 Views
  • 5 replies
  • 0 kudos

Throughput USB bulk transfert

Posted on July 15, 2014 at 17:29Hey guysI'm working on a projet and i'm using STM32f4 discovery board.I wrote program to send data by USB (from MCU to PC by Bulk transfert) in full speed mode.Usually the throughput should be 12 Mbits/s but mine is o...

DMA and SDIO problem (Solved)

Posted on March 06, 2014 at 22:33Hullo guys , ....... I got SDIO and DMA working fine , but now i want to use the DMA so store the data automatically into external SRAM for further processing , now the problem is that the documentation tells very fe...

ADC with DMA on different channels

Posted on July 16, 2014 at 10:33 I am using a F401 to read 1024 Samples with 40ksps and it works fine so I hope that the code is ok. DMA_INIT.DMA_Channel = DMA_Channel_0; DMA_INIT.DMA_PeripheralBaseAddr = (uint32_t)ADC1_RDR; DMA_INIT.DMA_...

lukas23 by Associate II
  • 2805 Views
  • 6 replies
  • 0 kudos

SDIO timeout

Posted on July 16, 2014 at 02:29 Hi! I have a small rtos and I have to write a string every 5 ms to a sdcard. This (pseudo)Code works fine: void SDTask(...){ // some init for( ;; ){ SDopen(&File); SDWriteString(&File,SDstr...

Real FFT CMSIS

Posted on July 14, 2014 at 15:38Hi,I am trying to do the FFT over an input real data (audio) on STM32F4 DISCO EVK & external CODEC. I have used the CMSIS function  arm_rfft_fast_f32() http://www.keil.com/pack/doc/cmsis/DSP/html/group___fast.html  I ...

dgetino by Associate
  • 1773 Views
  • 1 replies
  • 0 kudos

Receive data is wrong

Posted on July 12, 2014 at 11:17USART communication with stm32f4 discovery application did. At the beginning of the data sent to the PC comes an unwanted character. Sent from the computer to one of the characters I can not even. I changed it to HSE ...

How to sync clocks? - STM32F429

Posted on July 15, 2014 at 14:51Hi I am using STM32F429 with IAR work environment and i am trying to sync two clocks first clock: MCO2 is configured to output 29.5MHZ by using PLLI2SCLK second clock: LCD-TFT configured to output 14.75MHZ (half of M...

STM32F401 Discovery ADC tracing

Posted on July 15, 2014 at 22:16Hi, With the Keil qVision v5 Logic Analyzer I'm tracing (ST-Link) an single ADC value which is updated every 10 microsecond. Directly after starting the trace I get ''Trace: SW Buffer Overrun''. Is this a ST-Link lim...

paul2 by Senior
  • 1102 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.