STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Recieve more then 1 Byte over USART

Posted on August 31, 2012 at 20:51 Hi, at the moment I'm using the following code to recieve a byte: char ReceivedData = NULL; void main() { . . . while (1){ /* Wait until a byte is received */ while (USART_GetFlagStatus(USART...

sam239955 by Associate II
  • 20325 Views
  • 19 replies
  • 0 kudos

Stepper motor, timer phase control

Posted on August 07, 2014 at 23:26I am setting up stepper motor control on an STM32F4xxx using Full Step Drive as in http://en.wikipedia.org/wiki/File:Drive.pngBoth timers are setup as up counters with PWM output. Timer 2 controls phases A & C. Time...

picguy2 by Associate II
  • 1939 Views
  • 2 replies
  • 0 kudos

EXTERNAL RAM WITH STM32F429DISCO

Posted on May 14, 2014 at 09:37Hi!I would like to use the external RAM IS42S16400 present into the demo board STM32F429DISCO to store program variables. To do that i modify the linker script MEMORY{ FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048K R...

gerson74 by Associate II
  • 3323 Views
  • 8 replies
  • 0 kudos

STM32F2x documentation bug?

Posted on August 07, 2014 at 10:24Hello ST,I have found a discrepancy between the documentation of the STM32F2x MCU and the STM32Cube as well as the StdPeriph implemenation.On page 656 of the RM (RM0033_CD00225773, DocID15403 Rev 6) it is said that ...

RTP and STM32f107

Posted on August 07, 2014 at 19:59I use STM32f107 for audio broadcasting in ethernet network.I use trigged ADC (timer) to generate 8KHz PCM and buffer ADC data with DMA and make Alaw(G711,Fast conversation,table based) and send data with UDP. I use ...

Upgrade Project STM32F1xx UV2 to UV5 Error stdbool

Posted on August 01, 2014 at 16:52Hello,i'm Fabien and i'm a beginner with UV5 and STM32 and i need to modify a project but i have a 64bit windows so i need use UV5 with a new lib stm32f10x.h.I can change my project but i have a lot of error with th...

faza by Associate II
  • 3175 Views
  • 9 replies
  • 0 kudos

USB HS in FS + Internal DMA problem

Posted on August 07, 2014 at 16:36 Hi All, I have just started developing on the STM32 F4 Discovery with the purpose oftransferringdata from one incoming DMA (ie camera source) and out USB to a host PC. I have managed to get the...

Embedded distribution for STM32 series

Posted on August 07, 2014 at 10:38Hi. I have STM3210B-EVAL board which has STM32F10xxx microcontroller. I would like to know which could be the best embedded linux distribution for this microcontroller. Could I use Android on this board? I am not s...

shauns87 by Associate II
  • 1103 Views
  • 2 replies
  • 0 kudos

Porting BlueNRG Nucleo from F4 to L1

Posted on August 07, 2014 at 12:48Recently received the STM32 Nucleo BlueNRG board and got the code running on IAR with the F4 nucleo board, however I'd like to port the code to the L152 board. Is there a standard procedure somewhere to port from on...

johnlee by Associate II
  • 686 Views
  • 0 replies
  • 0 kudos

STM32F401 Nucleo, SDIO, TX FIFO UNDERRUN, CMD53

Posted on August 05, 2014 at 14:38 Hi,I am facing an issue with SDIO for STM32F401RE Nucleo platform,I am trying to use CMD53 data command. From the functions below CMD53_Start(), I get correct response, I have verified the response is valid.Howeve...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.