STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 minimal schematic

Posted on August 08, 2014 at 17:21Hello! I'd like to design minimal schematic for STM32F429. I'd like to have all pins connected to goldpins. I want to program through ST-LINK and SWD. Please check my schematic. It's in the attachment. Thanks! #s...

erazmus by Associate
  • 3336 Views
  • 6 replies
  • 0 kudos

DISCOVERY BOARD SPI NO NSS

Posted on September 01, 2014 at 06:25Hello, I have a Discovery board and am using the SPI master DMA example and SPI4. I set NSS as SPI_NSS_HARD_OUTPUT. What I get is CLK, and MOSI come out perfectly, but NSS is pinned low. I put a pullup on it, and...

david2399 by Associate II
  • 2432 Views
  • 4 replies
  • 0 kudos

Run the STM32 System bootloader from application?

Posted on September 03, 2014 at 17:26I've been trying to run the system bootloader from my application on an STM32F205.  I think that should b feasible, but at present the system firmware behaves badly.  Probably I'm doing something wrong, but I can...

STM32F4 PSRAM configuration

Posted on September 03, 2014 at 10:26Hello, At the moment I am designing a PCB with the STM32F4 and PSRAM. Are the FSMC_NEx signals the bank switch signals? Can I use all the FSMC_NEx signals for the PSRAM or are certain banks only for a certain me...

0690X00000602xTQAQ.jpg
ad23 by Associate
  • 1507 Views
  • 1 replies
  • 0 kudos

STM32F103VC with MMCCard

Posted on September 01, 2014 at 17:11Hi,I want to use 512 Mb MMC card with STM32F103VC.Hardware is ok . Do you have any ideas on this issue? any driver for STM.How can I read and write file in MMC card ? Regards,

nafb by Associate II
  • 2192 Views
  • 5 replies
  • 0 kudos

SPI DMA Problem, please help

Posted on September 03, 2014 at 00:58I'm trying to run SPI on DMA Mode for STM32F407 (Discovery). I'm stuck with the below code, with the oscilloscope showing SPI CLK but no data. I'm wondering:1. How do you do slave select in DMA Mode?2. Is the DMA...

Why does usb_bsp.h include stm32f4_discovery.h?

Posted on September 03, 2014 at 23:30The STM32F4-Discovery_FW_V1.1.0 library has USB code that I'm using in an STM32F4 project for USB HID support.  usb_bsp.h has the board support package function definitions.  I'm implementing these for my own cus...

avoid returning from interrupt

Posted on August 30, 2014 at 23:22Hi Forum, Is there any way to avoid returning from an USART1 interrupt? The booting process of our unit takes some time so we want to jump to the main menu quickly by pressing a key on the keyboard. This works and t...

stenasc by Senior
  • 2343 Views
  • 5 replies
  • 0 kudos

VREF+ not working as expected

Posted on September 03, 2014 at 19:53Greetings all -- I have a custom board built around the STM32F303VC, which has separate pins for VDDA and VREF+.  In the interests of keeping the voltage reference quiet, a 3.0V regulator is attached to VREF+, an...

aaron by Associate II
  • 1368 Views
  • 1 replies
  • 0 kudos

USB multiple CDC firmware

Posted on September 02, 2014 at 21:53Hi, I'm working with the STM32F40G EVAL board, and used the STCube to generate USB CDC middleware and it works fine. I am interested in modifying the STCube generated firmware, and having the device enumerate as ...

c_uimran by Associate II
  • 2328 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.