STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32Cube Memory Usage

Posted on September 03, 2014 at 19:43I created a very simple project targetting a STM32F042K6 processor.  It includes a USB Device with CDC class as the only Middleware selected.  No other items are enabled.  When I go to compile the STM32Cube outpu...

jon2 by Associate II
  • 4419 Views
  • 5 replies
  • 0 kudos

STM32Cubex and eclipse

Posted on June 02, 2014 at 17:27Hi,I am struggling trying to have a plain empty project to work under eclipse from STM32CubeMX generated code.  Why is there is no option to generate code for eclipse?  What is the procedure to migrate from a project ...

sine generator per AN3126

Posted on September 08, 2014 at 03:06I'm using an STM32F439 up clocked at 168 Mhz. I want to generate a sine wave exactly as outlined in app note AN3126 but I have several questions. 1) In the App note paragraph 2.1.3 it talks about the frequency of...

F103 HSI instead of HSE

Posted on September 06, 2014 at 17:52 hello dear forum, I have changed F103 on the motherboard - however, HSE doesnot start up but I can download code into the F103 with USART I dont want to throw away the board my...

The I2C doesn't work! (STM32f030 and STM32f103)

Posted on September 02, 2014 at 18:54Hi ST partisans! (Wink) I have written two program for my two MCU. STM32F103RET6 and STM32f030. in the circuit, the STM32F030 should send ''Rohalamin'' string over I2C (as Master) . on the other hand, the STM32F1...

stm32f030: PF0/PF1 as GPIO

Posted on September 06, 2014 at 08:50 Dear forum members, I hope you can help solving a mystery. I stumbled upon these cute stm32f030f4 µCs and built minimalistic boards with it. No external oscillator used, thus pins PF0 and PF1 should b...

0690X00000602xiQAA.jpg
de_koepi by Associate II
  • 2270 Views
  • 1 replies
  • 0 kudos

STM32F4 SPI & Busy state

Posted on September 06, 2014 at 04:45Hello, I'm trying to handle the Chip Select pin via software, but I can't figure out how to determine when the SPI peripheral has finished the current transfer. By the looks of it, the SPI_SR_BSY flag, becomes 0 ...

shopping by Associate II
  • 774 Views
  • 0 replies
  • 0 kudos

STM32F411 VREF+ and VDDA Pinout Question

Posted on September 06, 2014 at 02:07Hello all,I am trying to confirm the pinout for Vref+ and VDDA on the STM32F411 products. The datasheet states if Vref+ is not available it is internally tied to VDDA. Only the UFBGA100L and LQFP100 packages expo...

STM32F0 spi clock problem

Posted on September 04, 2014 at 12:29 Hi! I'm trying to communicate with Atmel AT45DB081D dataflash over SPI. For testing I've send command to read Manufacturer and Device ID (0x9F on MOSI). After I've sent data, SPI clock stops to pulse...

zlajoan by Associate II
  • 2183 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.