STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Combining Input Capture, One-Pulse Mode, and Reset Mode

Posted on October 07, 2014 at 16:28I am using an STM32F407xx.My setup is that I have TIMa triggering TIMb. Here is a description of the behavior that I want:TIMa:Don't care. This part looks to be working in my application.TIMb: When we get a Trig:...

dibs by Associate II
  • 1026 Views
  • 0 replies
  • 0 kudos

Bug in stm32f4xx_hal_nor.c

Posted on October 03, 2014 at 20:20In  HAL_NOR_GetStatus(..) timeout is not working due to an error:-----------------while(status != NOR_SUCCESS)  {    /* Get tick */    tickstart = HAL_GetTick(); // this should be before the while !!!    /* Check f...

Johanan1 by Associate II
  • 734 Views
  • 1 replies
  • 0 kudos

STM32 TRST

Posted on October 07, 2014 at 02:36I would like to use the Cortex M debug connector to debug and program an STM32F205.  The 10-pin connector does not have a JTAG TRST pin.  Will it still work with the STM32F205?  I plan to use an OCD debugger if tha...

STM32 Series - Calculations of Timer Variables.

Posted on October 05, 2014 at 04:02This is a subject that seems to have a lot of confusion (I do not fully understand). How to calculate the Variables: Period Prescaler Duration if only a few other variables are known. At higher frequencies, for e...

STM32Cube Tool Chains

Posted on October 06, 2014 at 22:18I downloaded, installed and used your STM32Cube software, Great Stuff, but when it came time to generate the code I was given a choice of :EWARM IAR MDK-ARM Keil TrueStudio Atollic Tool chains, where is the GNU too...

KevinA by Senior
  • 1153 Views
  • 1 replies
  • 0 kudos

STM32 sends weird characters to COM ???

Posted on October 06, 2014 at 17:36Hello, I send a char string to com port using sym32f4( with 3 pins only: GND VCC TX) and listen using ''hercules'' program finded on the net. I get weird characters, took a screanshot and uploaded as attachment. Ca...

aybala5 by Associate II
  • 8717 Views
  • 14 replies
  • 0 kudos

Mising startup file

Posted on September 23, 2014 at 01:44Hi All,I have done a search to no avail on this:Using Keil tools and Cube 4.3.1 (STM32F407), generating the project results in missing the startup file - but only at random.The folder ''Application/MDK-ARM'' does...

STM32CubeMx STM32F3 CCM-RAM

Posted on September 10, 2014 at 00:31Hi,  I would like to know if there are the option to create a IAR project in the STM32CubeMx that use CCM-RAM to run interrupt routines. If not. Are there plans to add it in the future?Ari.

Asantos by Senior
  • 718 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.