STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using TIM1 for SPI CLK

Posted on November 05, 2014 at 20:30I need to have 2xSPI synchronized and also synchronized with some timers.Unusual use of TIM1. (STM32F401VC, discovery board)I use TIM1 in repeat and one pulse mode to generate 8 CLK for 1 byte of SPII have a worki...

0690X00000604iRQAQ.png
stegu by Associate
  • 1682 Views
  • 2 replies
  • 0 kudos

STM Studio and elf file from GNU ARM eabi 4.8

Posted on November 01, 2014 at 12:03Hi all, I have issue with importing variables in to STM Studio 3.3. Import shows me only few variables (usually only uint8_t type), rest variables of different types (uint16_t, uint32_t ..) are not in list. Elf fi...

FPU comsums seeable extra power?

Posted on November 05, 2014 at 12:11Hi  everyone! I have a project where necessary to use FPU to proccess my AD data. If I enable the FPU in the uVision Keil, then I can see an extra noise on my power line and I get wrong values, but when I disable ...

Attila by Associate II
  • 4980 Views
  • 6 replies
  • 0 kudos

underclocking STM32F030

Posted on November 04, 2014 at 13:17I have problem when underclocking STM32F030. When I setup to RCC->CFGR2   higher value than RCC_CFGR2_PREDIV1_DIV4 (for example DIV5 - DIV16) then PLL is never ready ( RCC_CR_PLLRDY ) With value <= RCC_CFGR2_PRE...

How to know which timer triggered the callback

Posted on November 05, 2014 at 12:14 How can I check what timer triggered the callback: void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) { } I investigated the htim structure, but did not find anything that can be used to...

Displaying Bitmaps with STemWIN

Posted on October 08, 2014 at 00:01Hey,Im having a problem getting bitmaps to draw with the following functions:IMAGE_SetBMP()GUI_BMP_Draw()GUI_DrawBitmap()When drawing with any of these functions I see either the top-left most pixel or a vertical r...

craig23 by Associate
  • 1358 Views
  • 1 replies
  • 0 kudos

Question on STM32L USART communication

Posted on November 04, 2014 at 17:01I am using the STM32L1 Discovery Board (this one http://uk.farnell.com/stmicroelectronics/stm32l152c-disco/stm32l-discovery-eval-board/dp/2317987). I have written a program for USART communication on the two pins ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.