2014-11-01 4:03 AM
Hi all,
I have issue with importing variables in to STM Studio 3.3. Import shows me only few variables (usually only uint8_t type), rest variables of different types (uint16_t, uint32_t ..) are not in list. Elf file compiled by ARM GNU eabi 4.8 2014q2 from Coocox IDE same as map file shows address of all variables. I can read them to stm studio, but I have to fill variable address and size manually and after some modification in program I have to do it again. So I think that there is some noncompatibility between elf file and import method. Does anyone knows what to do to produce compatible elf file with stm studio?Elf file decoded header (part of it - variables are there)
[ 172] 08000919 00000002 FUNC WEAK 1 TIM6_DAC_IRQHandler [ 173] 08000129 00000018 FUNC GLOBAL 1 RCC_APB1PeriphClockCmd [ 174] 08000571 00000164 FUNC GLOBAL 1 PrepniStringy [ 175] 200000aa 00000002 OBJECT GLOBAL 3 VCSNapeti [ 176] 080000f9 00000018 FUNC GLOBAL 1 RCC_AHBPeriphClockCmd [ 177] 08000919 00000002 FUNC WEAK 1 EXTI2_3_IRQHandler [ 178] 08000919 00000002 FUNC WEAK 1 I2C2_IRQHandler [ 179] 08000a05 00000014 FUNC GLOBAL 1 DMA_GetFlagStatus [ 180] 08000919 00000002 FUNC WEAK 1 TIM17_IRQHandler [ 181] 08000919 00000002 FUNC WEAK 1 RTC_IRQHandler [ 182] 200000c0 00000000 NOTYPE GLOBAL 3 _ebss [ 183] 08000c79 0000007c FUNC GLOBAL 1 TIM_OC1Init [ 184] 080008cd 00000034 FUNC WEAK 1 Reset_Handler [ 185] 080004b9 00000060 FUNC GLOBAL 1 DMA_Config [ 186] 20000094 00000004 OBJECT GLOBAL 3 Timer [ 187] 20000098 00000001 OBJECT GLOBAL 3 Latch [ 188] 20000000 00000002 OBJECT GLOBAL 2 LastVDIM [ 189] 08000e90 00000038 OBJECT GLOBAL 1 CurrentTableMaxPart of map file (part of it - again variables are listed there):
*(.bss*) .bss 0x20000088 0x4 ..\obj\hw_config.o 0x20000088 SystemTimer .bss 0x2000008c 0x10 ..\obj\main.o 0x2000008c VstupniNapeti 0x20000090 StavLEDStringu 0x20000094 Timer 0x20000098 Latch *(COMMON) COMMON 0x2000009c 0x24 ..\obj\main.o 0x2000009c VrefInt 0x2000009e PredchoziNapeti1 0x200000a0 krk 0x200000a4 Timer200ms 0x200000a8 PredchoziNapeti1a 0x200000aa VCSNapeti 0x200000ac PredchoziNapeti2a 0x200000ae VCSResistor 0x200000b0 PredchoziNapeti2 0x200000b2 VDIM 0x200000b4 ADCDataValuesImported result in STM studio (complete - so except few variables everything is missing :( )
stm32f0xx_rcc.c (C:\Tomas\ARMC\LinearLedDriver\1\stm32_lib\src) APBAHBPrescTable[0] 0x0 unsigned 8-bit
hw_config.c (C:\Tomas\ARMC\LinearLedDriver\1\Source\src) Tlacitka[0].Stav 0x0 unsigned 8-bit
hw_config.c (C:\Tomas\ARMC\LinearLedDriver\1\Source\src) Tlacitka[0].Zmena 0x1 unsigned 8-bit
hw_config.c (C:\Tomas\ARMC\LinearLedDriver\1\Source\src) Tlacitka[0].PredStav 0x4 unsigned 8-bit
main.c (C:\Tomas\ARMC\LinearLedDriver\1\Source\src) Latch 0x20000098 unsigned 8-bit
main.c (C:\Tomas\ARMC\LinearLedDriver\1\Source\src) StavLEDStringu 0x20000090 unsigned 8-bit
main.c (C:\Tomas\ARMC\LinearLedDriver\1\Source\src) krk 0x200000a0 unsigned 8-bit
system_stm32f0xx_temp.c (C:\Tomas\ARMC\LinearLedDriver\1\cmsis_boot) AHBPrescTable[0] 0x20000074 unsigned 8-bit
#stm32 #stm-studio #gnu2014-11-04 8:16 AM
Hello,
The STMStudio was not validated with such elf file, so most probably the file is badly parsed. May you please post a little example (elf file only) for us to investigate ? Thank you ! Meanwhile, if your linker provides such kind of functionality, you might try to change the format for debugging information, just in case they are better parsed by the STMStudio v3.3. Best regards2014-11-05 5:52 AM
Hi SC,
I tried to modify format of elf file, but I was not successful. I attached some sample elf file. Thanks for your interest, Regards, Tomáš2014-11-05 7:33 AM
Hello,
Thank you for the elf file, it effectively shows a syntax not managed by STMStudio v3.3 and not faced with other supported compilers. Please find in attachment a beta version of a v3.4 fixing this (zip file with 2 jar files to extract in ''Program Files''\STMicroelectronics\STMStudio). Note that this version has not been validated, however modifications are localized. I hope this will help Best regards ________________ Attachments : STMStudioV3.4Beta.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzTJ&d=%2Fa%2F0X0000000bMJ%2FdF7VBk4GO21jpMA_YyJhkVjAxAwUEfWM7NvMooCCZrE&asPdf=false2014-11-05 7:47 AM
Hi SC,
thank you for your great support. Modified files work well. Best Regards, TomášWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.