STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429IG - USB FS Device mass storage + SDIO - not working

Posted on December 06, 2014 at 19:13Hello,I want use USB + SD SDIO. I used standard libraries from ST but I still get following messages:> MSC Interface started. USB Device Library v1.1.0 [FS] USB Device Library v1.1.0 [FS] > MSC Interface started. ...

198031 by Associate
  • 1715 Views
  • 3 replies
  • 0 kudos

Change CCR1 value with HAL

Posted on December 03, 2014 at 01:01Hi everyone,I'm starting with STM32 so i am running through some examples.I am using HAL since it helps porting codes between different MCUsI am now trying using PWM with the timer. I can't seem to find any functi...

Working Demos for STM32429I-EVAL?

Posted on December 05, 2014 at 20:24Hi folks,I'm working thehttp://www.st.com/web/en/catalog/tools/PF259093nd looking for working demos. It came with a demo loaded into flash (V1.1.1 IIRC) that was fully functional. Using the IAR EWARM tools I've bu...

hbarta2 by Associate III
  • 1262 Views
  • 2 replies
  • 0 kudos

STM32F407 I2S single DMA transfer size

Posted on December 05, 2014 at 01:14I need to make a single small TX transfer over I2S interface using DMA. But instead of short transfer I've got a long-long transfer (seems of maximum size). What is the right method to set the number of packets to...

shield

Posted on December 05, 2014 at 18:25Does ST Nucleo Board support competitors Shield from Arduino? Or any plan?

Bootloader

Posted on December 05, 2014 at 18:22Does ST provide a bootloader to just have USB interface for programming software without a programming tool?

STM32L Discovery Board - Touch panel

Posted on December 05, 2014 at 17:35Anyone knows a code to use the touch sense panel of the STM32L Discovery board.I mean a simple program that puts in a variable the touch position.Thanks

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.