How to check the FLASH integrity on STM32f103rct6
Hi @mƎALLEm , do you have any suggestions to perform the integrity check for the application stored in flash ? Best Regards, Aadesh
Ask questions, find answers, and share insights on STM32 products and their technical features.
Hi @mƎALLEm , do you have any suggestions to perform the integrity check for the application stored in flash ? Best Regards, Aadesh
Hello ST Support Team, Does the internal flash in STM32f103rct6 MCU supports the ECC feature? I am not able to find this information in related documents. Best Regards, Aadesh
I'm encountering an issue with the update event triggering in STM32 TIM1. I have configured TIM1 to generate PWM signals and set the update event to Center-Aligned Mode 3. However, I've noticed that the update event occurs not only when the timer's c...
Good afternoon,I am testing my UART and using a vector to store float numbers as shown below: raptor::std::vector<float> numbers; numbers.append(3.14f); numbers.append(2.21f); numbers.append(1.01f); numbers.append(8.15f); numbers.append(0.05f);H...
Dear Sirs,Is there a method to calculate the firmware size?I am using STM32F103R8T6My flash memory is divided in three blocks:- Custom boot loader block- Main application block- Data blockWhen the main application is running, it needs to calculate it...
I'm using Keil uVision 5 and ST-Link debugger (Mini). I have a very curios issue with STM32F746, running at 50 MHz.On the board I'm communicating with a display via FMC. "Suddenly" (as in, I don't know what I changed) the program did not work anymore...
I'm using the STM32H735 to create a sequence of PWM signals. I have timers TIM1, TIM2, TIM4, and TIM24 all connected in a slave timer chain. TIM1 triggers TIM2 with ITR0. TIM2 triggers TIM4 with ITR1, and TIM4 triggers TIM24 with ITR3. Each link in t...
Hi,1. Can the selected input channels to ADC0, ADC1 and ADC2 in STM32H753ZI be sampled simultaneously under the same sampling clock?2. NUCLEO-H753ZI ADC does not accept the analog negative signal inputs. Is there any STM32H7 dev board(s) accepting th...
I'm tring to work with a STM32F030F4. Unfortunately I didn't manage to flash the application on the controller. I'm using openOCD with a ST-Link.I use the following to start openOCD: openocd.exe -f interface\stlink-v2.cfg -f target\stm32f0x.cfgI now ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.