STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[SOLVED] STM32F205 DAC Speed

Posted on July 04, 2014 at 10:20I am using the code from the DAC with DMA example in the Standard Peripheral Library V1.1.0 to produce a sine wave. The updates seem to occur about every 4.5us. Is it possible to significantly increase the update spee...

sm23 by Associate II
  • 2410 Views
  • 5 replies
  • 0 kudos

STM32CubeMX freeRTOS

Posted on July 21, 2014 at 19:34Hi ,1. How Can i Find which version of freeRTOS the STM32CubeMX add to the project ?2. I don't Know if this the right place to ask , but does freeRTOS fully support     CMSIS-RTOS API ?  Thanks .

eyals111 by Associate II
  • 1752 Views
  • 2 replies
  • 0 kudos

SPI problem NucleoF401<->TI Launchpad

Posted on March 11, 2015 at 23:38 Hello, I am having a little problem with my SPI between the nucleo board and the TI cc3200 launchpad. I have been using the SPI communication without any problem under the following configuration ...

salman by Associate II
  • 1453 Views
  • 2 replies
  • 0 kudos

I2C_FLAG_BUSY problem

Posted on July 10, 2014 at 10:49Good morning,  I have some problems on I2C bus on STM32F1 micro. I have 8 prototipes board (all with the some mounting). 4 of those works fine and I can read and write the EEPROM on board (a 24xx series standard memor...

stefano23 by Associate II
  • 2240 Views
  • 2 replies
  • 0 kudos

USART2 interrupt continuosly fires

Posted on March 11, 2015 at 14:55Hello all,I have a problem with my USART2 interrupt on STM32L151.I have the USART_IT_RXNE, and USART_IT_TXE interrupts enabled on UART2. All other interrupts are disabled. The interrupt works fine until something wei...

srdjan by Associate II
  • 3443 Views
  • 11 replies
  • 0 kudos

my ADC code cann't get value

Posted on March 04, 2015 at 17:41The original post was too long to process during our migration. Please click on the attachment to read the original post.

LWIP ETHERNET PROBLEM

Posted on March 11, 2015 at 13:43hii used lwip example in stm32cubef4 like to(udp echo server,tcp echo server,......).when i connect 2 stm32f407 eval boards as udp or tcp servers to ethernet hub switch and connect to pc as client my servers don't wo...

osMailQDef error in cmsis_os.h

Posted on March 10, 2015 at 19:09The definition of the osMailQDef macro is incorrect in cmsis_os.h; it is missing a semicolon. Here is the original version: #if defined (osObjectsExternal)  // object is external #define osMailQDef(name, queue_sz, ty...

ccox by Associate II
  • 1173 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.