2015-03-10 11:09 AM
The definition of the osMailQDef macro is incorrect in cmsis_os.h; it is missing a semicolon. Here is the original version:
#if defined (osObjectsExternal) // object is external #define osMailQDef(name, queue_sz, type) \ extern struct os_mailQ_cb *os_mailQ_cb_##name \ extern osMailQDef_t os_mailQ_def_##name #else // define the object #define osMailQDef(name, queue_sz, type) \ struct os_mailQ_cb *os_mailQ_cb_##name \ const osMailQDef_t os_mailQ_def_##name = \ { (queue_sz), sizeof (type), (&os_mailQ_cb_##name) } #endif Here is the corrected version: #if defined (osObjectsExternal) // object is external #define osMailQDef(name, queue_sz, type) \ extern struct os_mailQ_cb *os_mailQ_cb_##name; \ extern osMailQDef_t os_mailQ_def_##name #else // define the object #define osMailQDef(name, queue_sz, type) \ struct os_mailQ_cb *os_mailQ_cb_##name; \ const osMailQDef_t os_mailQ_def_##name = \ { (queue_sz), sizeof (type), (&os_mailQ_cb_##name) } #endif2015-03-11 6:43 AM
Thanks Charles.
Reported issue will be fixed in coming releases of Cube packages.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.