STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f07+touch

Posted on April 09, 2015 at 17:40hello every onei want to connect touch panel to the adc of stm32f0 directlyso i use PA3->X+ PA4 ->Y+PA5->X-PA6->Y-pa5,pa6 just use as gpio and pa3,pa4 use as gpio and adc bothi config the adc first and defult channel...

Starting SPI master with DMA by an external signal

Posted on April 03, 2015 at 18:02I'm trying to read the serial data from two AD7766 (24 bit ADC in daisy chain mode) with a STM32F4 discovery board. The two AD7766 generates every 8 us new data. This is indicated by the ''Data Ready'' (DTRY) pin who...

freddy by Associate II
  • 1612 Views
  • 2 replies
  • 0 kudos

syscalls.c & uart.c

Posted on April 09, 2015 at 01:39Using gcc compiler with stm32f407 device FreeRTOS based FAT32 file system, Moment I remove uart.c and uart.h whole program halts nothing works. very strange its third day in debugging. Attached syscall.c and syscalls...

DMA request queue

Posted on April 09, 2015 at 06:10Hi all,I am working on an STM32F0 project in which I am triggering a DMA transfer using peripheral events such as an input capture. Looking over the docs it seems a little vague as to the behaviour of the DMA control...

luke2 by Associate II
  • 2006 Views
  • 2 replies
  • 0 kudos

STM32F4-DIscovery FAT example wrong

Posted on April 07, 2015 at 12:52In example:if(f_open(&MyFile, ''STM32.TXT'', FA_CREATE_ALWAYS | FA_WRITE) != FR_OK) Keil output: error:  &sharp167: argument of type ''char *'' is incompatible with parameter of type ''const TCHAR *''        if(f_ope...

chief by Associate II
  • 2552 Views
  • 5 replies
  • 0 kudos

About how to clear Pending Register

Posted on April 08, 2015 at 09:19Hello. I'm struggling with clearing pending register. I'm trying to clear the register in EXTI0 handler, but it looks like my program doesn't work. I'm using HAL driver, HAL_GPIO_EXTI_CLEAR_FLAG like below coding; HA...

Stm32f051 adc for multiple channels

Posted on April 07, 2015 at 09:14 Hello everyone, I have problem with the ad conversion into the stm32f051 microcontroller. My Destination is: AD-convert for multiple channels PC0, PC1, PC2, PC3, PB0 und PB1 My Problem: ...

STM32F373 SDADC common mode rejection ratio question

Posted on April 08, 2015 at 21:28Hello,I am interested in using the sigma-delta ADC on the STM32F373 microcontroller.  I would like to use it in differential mode to measure the output of a load cell bridge - but I have not been able to find any inf...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.