STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f334 ADC conflict

Hi all.Why when I configure an ADC input in PA2 port, I have a conflict with another pin PA3 port that is configured as GPIO?Many thanks. 

bestyeng_0-1733415071251.png
bestyeng by Associate II
  • 4521 Views
  • 6 replies
  • 1 kudos

Resolved! GPIO output in real life - STM32H7B3I-DK

Good morning, there is something i a not understanding well with my board. I need to use 10 GPIO as inputs of button or output. for that i went to the GPIO list, for example, I got GPIO at pin PI4 so I go on the schematics of my board and I see that ...

Capture d’écran 2024-12-05 à 15.35.14.png Capture d’écran 2024-12-05 à 15.34.44.png
Jad by Senior
  • 4377 Views
  • 9 replies
  • 10 kudos

USB on STM32H503

I'm having problems enabling USB on STM32H503 and I'm hoping there's a simple solution that you can point me to. The problem happens on both my custom board (STM32H503CBT6-based), as well as on MB1814B (STM32H503RBT6-based).  Here's the simplest repr...

romp by Associate II
  • 1663 Views
  • 1 replies
  • 1 kudos

Questions on how RTC clock usage STM32F103

I am planing to have a time functionality on a project I want to make.After reading the manual I undestood I have a 32 bit counter which increases with TR_CLK.Let's say I want to update the clock every 1ms, that would leave me with aproximately 49.5 ...

Resolved! Generate Tone Using DAC - STM32 NUCLEO-F410RB

Is possible to generate different tone using dac peripheral for triangle wave form generation using PCM sample in stm32 nucleo F410RB controller. Is it possible to generate tone using wav data(pcm array).1.If possible to generate need to give wav for...

AMS12345 by Associate III
  • 5443 Views
  • 12 replies
  • 4 kudos

Resolved! Operations on doubles with very unexpected results

Hi all,I am stumped with an issue that looks trivial but apparently isn't really ?This code... :double TMP117ConvertTemperatureToCelsius(uint16_t temperature) { double temp_double = (double)temperature; double multiplied = (double)temp_double * 7.8...

4lchemist by Associate II
  • 3150 Views
  • 7 replies
  • 1 kudos

Resolved! STM32H745 DAC2 missing

Hi, I would need dual DAC using STM32H745. According to datasheet, it should have two DAC converters. In STM32CubeIDE, I can see only DAC1 with two channels. In the datasheet, I can only see DAC1_OUT1 and DAC1_OUT2 pins, but no DAC2 out pins. Is ther...

mosamasa by Associate II
  • 3349 Views
  • 8 replies
  • 2 kudos

STM32U5 RTC calibration process

I am currently working with an STM32U5 microcontroller and would like to request more information on the process of calibrating the RTC (Real-Time Clock). We are using an external 32.768 kHz LSE oscillator with 10pf burden capacitors, but we are obse...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.