STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDRAM-based heap initialized as part of ZI-data

Posted on June 11, 2015 at 04:34 I'm developing an application which requires the heap to be located in a large off-chip SDRAM. I'm using Keil uVision5 and scatter-loading to accomplish this. Functionally, all is good and works as expected. ...

cnicolls by Associate
  • 737 Views
  • 0 replies
  • 0 kudos

USART System Bootloader - STM32L151xx

Posted on June 08, 2015 at 22:05Hello,I'm trying to use the default bootloader of this STM32L151CCT6 over USART1.I've read and follow all the tips and tutorials of AN2606 and AN3155, but without sucess.This is my process to try a communication: Tu...

uilter by Senior
  • 3734 Views
  • 10 replies
  • 0 kudos

How to reduce FLASH noise on STM32F205VET6?

Posted on May 28, 2015 at 23:12Hello! I am work with uC STM32F205VET6. Its flash is very noisy! How to reduce this noise with software methods? I tried turn off HSI, prefetch and slowdown core clock. Also I turned on spread spectrum clock generation...

usb ESD protection in stm32f4discovery

Posted on June 09, 2015 at 13:42HelloThe OTG side of the stm32f4discovery is ESD protected, but there isn't such protection in the STLINK side, why?How can we decide whether to put ESD protection IC or not? 

timer in HAL - prevent auto-disable

Posted on June 10, 2015 at 13:56What is the best way to prevent __HAL_TIM_DISABLE being called when all the CCxE are 0 ? __HAL_TIM_DISABLE(htim); is called in virtually every TIM...._Stop function It would be useful to keep the counter running parti...

pbayton9 by Associate III
  • 776 Views
  • 0 replies
  • 0 kudos

Bluetooth module echo problem

Posted on February 10, 2013 at 20:24 Hello, i am working on labview communication with bluetooth module driven by STM32F4, and some how i can't make it work. I can easy send data to labview, but not other way around, i have no idea where pro...

linas2 by Associate II
  • 3967 Views
  • 11 replies
  • 0 kudos

Stm32F4Discovery and AK4556 audio codec

Posted on January 28, 2015 at 14:08 I’m having a problem with my project. The project is just a simple sound “loop�? It is a stm32f4discovery connected to a audio codec. They communicate over I2S3 in Full Duplex mode and the stm...

0690X00000602tYQAQ.jpg 0690X00000602tcQAA.jpg
rasmus by Associate II
  • 3044 Views
  • 5 replies
  • 1 kudos

SPI - one-way communication Slave->Master

Posted on June 09, 2015 at 10:54Hello everybody, In my current project I need to establish an SPI connection between an STM32F407 microcontroller (slave) and an AD7763 A/D converter (master). Before the ADC actually starts sending any data, its two ...

Powf (power exponent) don't return float values

Posted on June 08, 2015 at 13:03 Hi everybody, I use the function powf (that is supposed to return a float), included in the library #include <math.h> This is the definition of the function in math.h : float powf _PARAMS(( f...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.