STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32F0 sd Card FATFS

Posted on June 28, 2015 at 14:49Hi I am using stm32f0 to wtrite and read from sd card using FATFS.Every thing is ok  : integration of FATFS files and making the correct hardware connection.I can communicate with the sd card for example to get its p...

Cesar cfg by Associate II
  • 2342 Views
  • 5 replies
  • 0 kudos

Bit-band - via a linker.

Posted on June 29, 2015 at 00:33Can anyone come in handy ...Code for linker GCC.xxx_sram/flash.ldMEMORY{    ROM  (rx) : ORIGIN = 0x08000000, LENGTH = __    RAM (rwx) : ORIGIN = 0x20000000, LENGTH = __    BITRAM (rw) : ORIGIN = 0x22000000, LENGTH = 2...

Setup FREERTOS with CubeMX

Posted on June 27, 2015 at 23:20I used CubeMX to setup FREERTOS on STMF0m Discovery board, with STM32F051R8Tx I keep getting Error 272: undeclared identifier ''SystemCoreClock Any suggestions how to fix that? Any help appreciated

gerhard by Associate II
  • 2276 Views
  • 4 replies
  • 0 kudos

SPI with DMA on STM32F437

Posted on June 23, 2015 at 15:39 Hi, I'm having troubles setting up the DMA with SPI2 on a STM32F4 I am using the streams 3 and 4 on channel 0 as said in the datasheet. Here is my init code : void MX_SPI2_Init( void ) { DMA_InitTyp...

alexpes59 by Associate II
  • 1682 Views
  • 3 replies
  • 0 kudos

STM32Cube and GCC for VCP

Posted on June 14, 2015 at 06:26I have the STM32F429 Discovery board and I am trying to get the Virtual Com Port working. I am using the GCC plugin for Eclipse, which can generate a blinky program that compiles and works for the board. I can also us...

Weird I2C problem stm32f4 switch 230V coil

Posted on July 22, 2013 at 14:02Hello everybodyI have the weirdest problem on my i2c....I have some pcf8574's connected on my stm32f4Discovery and the work like a charm(thanks Clive1.....)But now i have connected some 5V relays which also work fine ...

kenny__84 by Associate II
  • 7471 Views
  • 15 replies
  • 0 kudos

SPI FLASH read/write problem

Posted on July 21, 2013 at 13:50 Hello, i am making adsp-21488 spi flash programmer, and i run into some trublmes. I use STM32F415 and using SPI1 (PA5/6/7) *** PB0 for communication with SPI. I can read Flash ID with no problem, and it's...

_legacyfs_online_stmicro_images_0690X00000604zb.png

OV7670 with stm32f4-discovery?

Posted on January 11, 2013 at 18:51I have a project with OV7670 with stm32f4-discovery. My OV7670 has 16 pins and without fifo. And I don't have LCD. I hope I can use OV7670 to get view into stm32f4 and transmit data to smart phone and get the real ...

ctc.ctc by Associate II
  • 2266 Views
  • 5 replies
  • 0 kudos

OV7670 camera

Posted on February 15, 2012 at 08:55Good day,I have some problem here, I took some code from another project, I rewrote some parts. But my camera do not want to work. I just want to read the ID of camera through I2C (or so called SCCB), but I always...

hitsumen by Associate II
  • 2813 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.