STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer 8 of STM32F4 Discovery don't work !

Posted on March 11, 2013 at 10:54Hi,I have problems with Timer 8 this time. I want to measure the frequency of an input signal. I have to use PB1 that's connected to TIM8_CH3N. The code seem correct but it doesn't give any frequency. The code is the...

DSP functions on System Workbench and CubeMX

Posted on July 04, 2015 at 15:46 Hi, I'm trying to setup a project using System Workbench and CubeMX on an Nucleo Board (411RE). Could someone tell me a step by step on how to do that? I have an example fromSTM32Cube\Repository\STM32Cube_F...

stm32f0 discovery board to run One Pulse Mode on timer 2

Posted on July 09, 2015 at 22:13Hi, I am using the discovery board to try OPM on timer 2. I can not get it going with any effort on my code list below. Please help!!! It is important to our new product.void GPIO_Configuration(void);int main(void){  ...

ming2 by Associate III
  • 2049 Views
  • 5 replies
  • 0 kudos

I2C problems with STM32L Discovery

Posted on July 10, 2015 at 18:25I am trying to communicate with a ADT7410 I2C temperature sensor using a STM32L Discovery Board (PB6 for SCL and PB7 for SDA).I configure the I2C with the following code:void I2C_initialization(void){  I2C_InitTypeDef...

Baud Rate problem

Posted on July 09, 2015 at 17:15  The original post was too long to process during our migration. Please click on the attachment to read the original post.

fiulala by Associate II
  • 1326 Views
  • 4 replies
  • 0 kudos

Stop code execution during 8 timer interrupts

Posted on July 03, 2015 at 14:14Hi everyone, I'm working with the stm32f405 microcontroller and I am trying to send some characters using a simple GPIO pin. My problem is that I have to send each bit of one character every 20ms. For that I use a ti...

mnemxys by Associate II
  • 1474 Views
  • 2 replies
  • 0 kudos

Workshops at home

Posted on July 09, 2015 at 14:02Hi everyone,I was wondering if there are any workshops from ST that can be done at home. Something like PDFs with explanations and some exercises that you can do. More specifically for the standard peripheral library ...

SPI Bus Fault due to xPortSysTickHandler FreeRTOS

Posted on July 10, 2015 at 13:10When the xPortSysTickHandler is called at the moment the SPI HW block is executing a SPI communication the i get a Bus fault resulting in a Hardfault Is this a known issue? I can solve the issue by first executing the...

ronny by Associate
  • 753 Views
  • 0 replies
  • 0 kudos

L3GD20 gyroscope value drift on STM32F3-Discovery

Posted on July 10, 2015 at 13:08Using a D/A the converter I am now able to monitor the gyroscope rotational accelration around the x axis as a voltage. I run the gyroscope at 190 Hz rate and read the oscilloscope in a thread every time the the DRDY ...

STM32F405 PLL: 168MHz to 84MHz - how to do this?

Posted on July 08, 2015 at 05:07Hello: I have an STM32F405 processor, with a 8MHz HSE crystal. It's set up to operate at 168MHz. To see if I can get suitable performance at a lower speed to save power, I'd like to change this (*not* on the fly) at t...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.