STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cortex M4 check and clear instruction?

Posted on July 07, 2015 at 22:32 I'm using FreeRTOS on STM32F4 with ARM-GCC and i need to do some interrupt/task protection for a simple flag checking and clearing function. Here's an example: int flag; // Some code sets flag to 1 som...

Issue with Timer Input capture delta value on STM32F4

Posted on July 11, 2015 at 17:46 Hell all. i encounter some problems when trying to read the lenght of a pulse (low-hi-low) The ideea is the followin. I have a flag wich is set 5, then at the first falling edge in cc2 event, ...

Bogdan by Senior
  • 694 Views
  • 1 replies
  • 0 kudos

STM324xG_EVAL microphone (MP45DT02) problem

Posted on July 11, 2015 at 06:36I want to use ST MEMS microphone (MP45DT02) on STM324xG_EVAL board, I used an extension board and attached the digital microphone to the board. It works very well when I use 16 KHz for AudioFreq, I mean:#define DEFAUL...

rizzo by Associate II
  • 608 Views
  • 0 replies
  • 0 kudos

Set a flag to test after reset

Posted on July 11, 2015 at 00:11Hi folks,In my quest to leverage the built in bootloader I am employing code kindly provided by Clive to branch to the built in bootloader on the STM32F429I (As in/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat...

hbarta2 by Associate III
  • 1148 Views
  • 1 replies
  • 0 kudos

Scheduling future interrupts with a specific delay

Posted on July 09, 2015 at 01:12I'm trying to schedule a single interrupt in the future with a specific delay on the STM32F407, and I'd like to figure out the best way of doing this. I've played around with periodically waking up a task and generati...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.