STM32 Audio processing SW library
Posted on July 16, 2015 at 07:15Great to hear about that library, but some project examples will be useful.
Ask questions, find answers, and share insights on STM32 products and their technical features.
Posted on July 16, 2015 at 07:15Great to hear about that library, but some project examples will be useful.
Posted on July 16, 2015 at 03:57 I'm using the HAL drivers for the first time and I'm trying to implement the UART protocol. I used the stm32f74g... examples for the UART and copied part of the uart-polling example. The problem I get is t...
Posted on July 15, 2015 at 13:15Hi there, I'm going to ask quiet an odd question , is it possible to program an other microcontroller (a pic) using an stm32f4 disco or st link in general. I hope someone can answer me.Many thankx !
Posted on July 09, 2015 at 22:17Hi All,I'm trying to drive some WS2812 LEDs which require a (400ns high + 800ns low) or (800ns high + 400ns low) signal to indicate a 1 or a 0.So esentially I'm trying to take an array of data and output it directly t...
Posted on July 14, 2015 at 23:53Is the filter for the CAN ''Networking'' demo configured to accept all CAN frames? #stm32 #can #example #code
Posted on July 15, 2015 at 15:25Hi all, I am using a STM32F103VEH MCU which controls an external PN512 (NXP semiconductors) NFC RF reader. The MCU and PN512 communicate over a 8-bit bidirectional parallel interface as databus to exchange information...
Posted on July 15, 2015 at 09:22I have recently got my hands on an STM32F4Disovery board for one of my project requirements. I am supposed to use it with a transceiver and be able to transmit packet. Although I have done a bit of programming, it is ...
Posted on July 10, 2015 at 20:59Hello ST developers,I still don't know why I switched to HAL drivers (probably because there is no STD drivers for F7 lines) but I read MANY, MANY bugs in HAL library for F4 and after starting developing generic libra...
Posted on July 15, 2015 at 14:02I have a STM32L151UC, I am compiling a project getting a Hex and and Elf file, I flash the Hex file using ST-Link Utility and St-Link/V2 and I can start it on debug mode over openocd and gdb, being able to print with ...
Posted on July 15, 2015 at 16:12Hi I have adapted the program found below from the example 7PWM_Output in the StdPeriph library examples. My aim is to create 3 PWM channels each with it's respective complimentary output as well as inserted dead time...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.