STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F0 CAN self-reception?

Posted on July 10, 2015 at 23:59I'm using an STM32F0 for a CAN application. I noticed, though, that the MCU doesn't receive the messages that it sends out on the bus. It would be preferable for me to be able to see all of the data on the bus, though...

esimon by Associate II
  • 3424 Views
  • 6 replies
  • 0 kudos

How to attach TI CC1200 with STM32F4Discovery

Posted on July 16, 2015 at 17:04Hi,  I'm planning to attach CC1200 EMK with STM32F4Discovery kit on the SPI interface. I guess the best interface would be SPI for the same since I don't need the MEMS.  Could you please advise  how to make the hardwa...

Cortex M0 Vector relocation issue

Posted on February 07, 2014 at 00:42Hi, I'm trying to implement IAP on an stm32f051 device, but get a linker error when specifing VectorTable address is 0x20000000. __IO uint32_t VectorTable[48] __attribute__((at(0x20000000))); STM32F0-Discovery_Dem...

stenasc by Senior
  • 4423 Views
  • 10 replies
  • 0 kudos

output of DAC to input of ADC

Posted on July 16, 2015 at 15:52Good Afternoon Everyone,  Is it possible that on STM32F4 , I first do a DAC and then use its output as input to ADC and finally get a digital output ? If I can do that , how can I do this connection in between the DA...

nemisha by Associate II
  • 1114 Views
  • 1 replies
  • 0 kudos

New Release Raisonance Tools for STM32 [UPDATE]

Posted on January 14, 2015 at 17:48New release of Raisonance tools for STM32 is now available with support of new MCU variants in STM32 L4, F3, F4 and F7 lines. This software supports both the RLink and ST-Link debugger/programmers.The support Rais...

STM32F103 TIM PWM on CH2N only

Posted on July 15, 2015 at 12:29Hello,I have configured only PB0 (TIM1_CH2N) for PWM output, but I can't get any signal from the pin. code looks like this:  RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB | RCC_APB2Periph_AFIO | RCC_APB2Periph_TIM1, ENA...

How to sprintf an uint32_t value

Posted on July 16, 2015 at 11:43 Hello everybody, Amateur question: I search for a long time how to sprintf a 32bit value in a string. If I use sprintf (string_to_write, ''%u'' , uint32_value); The value is cropped as a 16 bit...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.