STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 - SDRAM - Byte enable

Posted on July 27, 2015 at 10:54Hello, i use a STM32F439 controller with 32Mbyte external SDRAM. I would like to configure some settings with STCube. There is a tab FMC with a sub-tab SDRAM1. When i select Data: 32 bits i can choose either Byte ena...

STM32L152- sometimes problems with wakeup

Posted on July 23, 2015 at 15:30After working our instrument goes in the sleep-mode (__WFI) to save power. With a key, which is connected to the Wakeup-pin, we can switch back in the operation mode. Sometimes this function does not work. In this cas...

STM32F7 Systick question

Posted on July 20, 2015 at 10:20 Hello, Right now i am try to remake my project for STM32F7 from STM32F4. HAL is just paint to work, i was unable to figure out what i have to write to functions to make it hal compatable, so instead i have to...

STM32CubeMX init hang on ETH STM32F4/DP83848

Posted on July 26, 2015 at 21:49In a STM32F427/DP83848 PCB configuration, I am finding that the LWIP/Ethernet initialization is hanging at a statement waiting for the Software Reset to clear. What specifically is the Ethernet MAC engine awaiting ? I...

STMCUBE mx - STM32F051 IAR EWARM tool chain

Posted on July 25, 2015 at 04:31I am just getting started with the Cortex (and C.)I would like to access an entire GPIO port but cannot find a way to address the port(GPIOF.)  I see the HAL functions for addressing the bits but not the entire port.H...

Connecting STM32F107 with DP83848 ??

Posted on July 25, 2015 at 13:11 Guys, I tried to interface STM32F107 and DP838... The code is generated from STM32CubeMX void HAL_ETH_MspInit(ETH_HandleTypeDef* heth) { GPIO_InitTypeDef GPIO_InitStruct; if(heth->Insta...

Problem with HAL_Init()

Posted on July 10, 2015 at 17:18Hi, I am kind of new to the STM32 but have found the libraries (HAL) to be greatly useful. I am using the STM32F4 Discovery Board, Even when I was trying to simply blink the onboard LEDs using the GPIO Peripheral, it ...

seprac by Associate II
  • 9322 Views
  • 10 replies
  • 0 kudos

STM32f407 MCU two interrupts at some time

Posted on July 25, 2015 at 02:13I used TIMER 2. It's interrupt time is 1us.I made one long pulse and short pulse using GPIO output pin and TIMER 2.but sometimes, interrupts occurred two times.First figure is the result I want to get.Second figure is...

ciel076 by Associate II
  • 2209 Views
  • 2 replies
  • 0 kudos

Disabling a particular IRQ in code

Posted on July 25, 2015 at 01:10I'm developing a custom CAN bridge with the stm3210c-eval board, such that I can hook up the board's CAN port to a car's CAN bus and the USART port to a computer and read in received frames over a serial terminal. In ...

bhargava by Associate II
  • 1104 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.