STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flash page erase problem. stm32f103vb

Posted on August 11, 2015 at 18:26Im having an issue erasing pages of flash. During my bootloader application while receiving a block of data I erase the page and then write the data. During testing I have the messaging protocol setup to just read t...

USART example code for Nucleo F401RE

Posted on March 26, 2014 at 04:16 Via Virtual COM port built into ST-LINK // STM32 USART2 (Tx PA.2, Rx PA.3) STM32F401RE NUCLEO - sourcer32@gmail.com #include ''stm32f4xx.h'' /**********************************************************...

SPI Status Flags Don't Update

Posted on August 09, 2015 at 20:09 I'm sitting here pulling my hair out because I can't figure out what's going on, I've tried everything I can think of. I'm using SPI to communicate with an offboard periph, When I write to the data register the...

Use of the same port both input and output

Posted on August 06, 2015 at 13:19 Hello, I need use a port both input and output. What should I do? Should I use something like this? GPIO_InitTypeDef GPIO_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); GPIO_Ini...

fenice-6 by Associate II
  • 4856 Views
  • 8 replies
  • 0 kudos

PCROP protection

Posted on March 20, 2015 at 16:30 For our customer I need build a new hw with a ST micro (STM32F4) with a pre-porgrammed code library. The client develops its own application using the preloaded library (Obviously I provide also all the necessa...

Circular DMA data looks like rubbish

Posted on August 11, 2015 at 11:28 Hi, I'm using DMA with Timer2 input capture to sample the (ch2)rising and (ch1)falling edges of a 250kbps signal. So a bit is 4us long. When running the DMA in normal mode, the values make sense a...

STM32F0 and usart

Posted on August 09, 2015 at 23:03Hello,Im want to send data with USART2 (im using KEIL uVision 5).Im trying to use this program :/* USART2 PA.2 Tx, PA.3 Rx STM32F0-Discovery sourcer32@gmail.com */ #include ''stm32f0xx.h''#include ''stm32f0_discover...

edouard by Associate II
  • 1559 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.