2015-08-09 2:03 PM
Hello,
Im want to send data with USART2 (im using KEIL uVision 5).Im trying to use this program :/* USART2 PA.2 Tx, PA.3 Rx STM32F0-Discovery sourcer32@gmail.com */ #include ''stm32f0xx.h''#include ''stm32f0_discovery.h'' int main(void){ USART_InitTypeDef USART_InitStructure; GPIO_InitTypeDef GPIO_InitStructure; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2,ENABLE); GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_1); GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_1); /* Configure USART2 pins: Rx and Tx ----------------------------*/ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USART2, &USART_InitStructure); USART_Cmd(USART2,ENABLE); while(1) { while (USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET) USART_SendData(USART2, 'X'); }}Im using Keil in simulation mode, and when i want to debug it, i add the USART2 register to check it and it says : <cannot evaluate>, when i run the program, it says : *** error 65: access violation at 0x00000000 : no 'execute/read' permissionBasically, I would like to check the USART2 register to see if I do have X in this register. Thanks for your help2015-08-09 3:11 PM
Ok, well this basically means that the simulation doesn't support the features of your part at the level you want to use them. Use the debugger on real hardware.
2015-08-11 5:01 AM
correct Clive1
Seehttp://www.keil.com/dd/chip/6188.htm
Simulated Features
NOTE
Simulation for this device is provided by the default peripheral simulation driver. Complete peripheral simulation is not available and is not planned to be implemented by ARM.To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.