STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Setting interrupt ADC conversion is complete using HAL

Posted on August 05, 2015 at 11:37STM32F407VG When Interrupt function looks like this:void ADC_IRQHandler(void){adc=HAL_ADC_GetValue(&hadc1); HAL_ADC_IRQHandler(&hadc1);  HAL_ADC_Start_IT(&hadc1);}Everything works well.But when I want to do the ADC ...

Fatal error: ST-Link, no MCU device found session aborted

Posted on August 10, 2015 at 11:26Hi When I configure the I2C to my code, my code is only using TSC, RTC, timer2 and sixteen GPIO. I compiler it that variable parameter is became ''unavailable'' in live watch windows. After that, I want to leave deb...

countach by Associate II
  • 4775 Views
  • 7 replies
  • 0 kudos

PWM with 1.5 MHz with STM32F411 Nucleo-Board

Posted on August 12, 2015 at 09:24Hello,i'm glad to be a member here in this forum. At the moment i am thinking about to buy a STM32F411 Nucleo-Board.  In this case i would like to ask you some question about this Board. I read many different articl...

mirco2 by Associate
  • 1927 Views
  • 2 replies
  • 0 kudos

HAL Vs Firmware

Posted on August 11, 2015 at 14:22Can anyone help me in understanding difference between HAL and firmware,I can find plenty of examples useful for starter as complete project in HAL related stuff, while no such thing available for firmware stuff (at...

waheed901 by Associate II
  • 3275 Views
  • 8 replies
  • 0 kudos

STM32L151 LSI clock accuracy

Posted on August 12, 2015 at 10:54HiRM0038 Reference manual sais: ''LSI clock ... The clock frequency is around37 kHz.''Can you tell me what is the max possible clock Deviation? (in percentage / Hz)ThanksYaron #stm32

yarona by Associate II
  • 2955 Views
  • 6 replies
  • 0 kudos

Undefined identifiers in .ini file

Posted on August 12, 2015 at 13:51 I trying send characters to the UART in simulation in Keil MDK-ARM using .ini file. This code is from uVision Help. signal void serialA_Z ( void ) { char ch; for (ch = 'A' ; ch < 'Z' ; ch++) { S0IN...

0690X00000604rwQAA.png
hospodar by Associate III
  • 1019 Views
  • 0 replies
  • 0 kudos

STM32F4 Memory organization

Posted on August 11, 2015 at 22:20Hello everyone!I'm beginer in STM32 MCU (I train on STM32F429-Discovery board). I couldnt find ansver for my question in Reference Manual and Programming Manual.In Programming manual ask that CODE memory space (0.5G...

kuzas by Associate
  • 4256 Views
  • 3 replies
  • 0 kudos

STM32CubeF4 is wrong version

Posted on August 06, 2015 at 21:01The current download claims to be version 1.7.0, but in fact it’s version 1.3.0.What would be really nice would be for all the versions to be available, so that we can select which one we want!

STM32F042F4: using PA11 and PA12 as IO

Posted on August 11, 2015 at 14:20 I'm trying to use PA11 and PA12 on a TSSOP20 STM32 as output to understand how this remapping and configuring works. Until now I'm unable to get it to work, the pins do not toggle. Can someone point me ...

bastiaan by Associate
  • 1301 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.