STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F042 SWD IDCODE error

Posted on August 22, 2015 at 21:51I have a problem with debugging an STM32F042 board. When the debugger (ST Nucleo) asks for IDCODE, the MCU responds with an error (trace shown below). At first, I thought that the bootloader is the problem, so I fla...

0690X00000605IdQAI.png
atx by Associate II
  • 1097 Views
  • 2 replies
  • 0 kudos

Display orientation in STemWin526

Posted on August 24, 2015 at 21:17Hello!I need help.I need to use vertical orientation of display.I use demonstration from STM32F429I-Discovery.I try to use combination #define COLOR_CONVERSION_0 GUICC_M565 #define DISPLAY_DRIVER_0   GUIDRV_LIN_OSY_...

STM32F405 Odd DFU behaviour

Posted on August 18, 2015 at 16:47I'm experiencing some odd behaviour when attempting to place an STM32F405 into DFU mode. Currently, what works on one peice of hardware is that is that I send the STM32 a command to tell it to go into DFU mode, and ...

Audio stream STM32F4 disco

Posted on August 24, 2015 at 11:48The original post was too long to process during our migration. Please click on the attachment to read the original post.

matas by Associate II
  • 889 Views
  • 1 replies
  • 0 kudos

STM32CubeMX - Missing pins in MX_GPIO_Init

Posted on August 18, 2015 at 00:11 I'm having a problem getting all the pins to show up in the generated code from STM32CubeMX. Here's what I'm seeing: I'm generating a project using STM32CubeMx (v4.9.0) for the STM32F3348DISCOVERY board...

tristan2 by Associate
  • 1343 Views
  • 1 replies
  • 0 kudos

.

Posted on August 22, 2015 at 19:18. #sai-audio-codec #stm32f7

Frequency Measuring

Posted on August 20, 2015 at 15:26Hi ,Please i have to measure frequency from 1Hz to 3Khz with timer 1 (16bits)My SysTick clk = 72Mhz, so i set the prescalor to (1000-1) .So i have a Counter Clock=72Kand than i can capture frequency starting from 1H...

nechi by Associate III
  • 2190 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.