STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIO configuration primer under STM32CubeMX

Posted on August 22, 2015 at 04:11Is there a document that describes the selection of push pull, open drain, maximum output speed, AHB clock, etc   for GPIO port operation  on STM32F427xx under STM32CubeMX ? The datasheets for the chips on the PCB t...

mkbrown32 by Associate II
  • 2154 Views
  • 5 replies
  • 0 kudos

SDIO microSD speedup

Posted on August 25, 2015 at 13:16Hey I am making a microSD card logger, it is going to run on a battery so the power  consumpion is of big importance and because of that microSD card speed also matters a lot. I've found the program H2testw which is...

matas by Associate II
  • 1195 Views
  • 3 replies
  • 0 kudos

STM32Cube improve config parameter UI

Posted on August 06, 2015 at 02:56Having to enable the description of the config parameters at the bottom of the window is non-sense.  there is plenty of room to add these in columns without taking any more space and will make it easier to browse fo...

ETM Trace on STM32F429

Posted on August 21, 2015 at 09:26Hello,I wanted to know if someone has already worked on ETM trace on STM32 cortex-M4. My purpose is to activate them into the embedded software itself and dumping traces on the 5 following pins (TRACED[0-3] + TRACEC...

STM32 ADC1 regular + ADC2 and ADC3 in injected mode

Posted on August 24, 2015 at 22:57Hi All,I've some problem configuring the ADCs of a STM32F407.I have 2 motors connected to my board that I drive with 2 different pwm.For the 1st motor I use a pwm from PE9 (TIM1 CH1)For the 2nd motor I use a pwm fro...

canta76 by Associate II
  • 1877 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.