STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 QUAD-SPI clock

Posted on September 04, 2015 at 17:17Hi, Based on the STM32L4 datasheet the maximum QSPI clock is 48MHZ, but the clock used for the cube examples is 80MHZ. should I reduce the clock to 40MHZ? I'm using the Spansion S25FL127S memory in my custom boar...

Asantos by Senior
  • 1314 Views
  • 2 replies
  • 0 kudos

STM32F072RBT6

Posted on August 24, 2015 at 11:15Hello, Can anybody help in order to setup the USART1 on this controller? I have a ST NUCLEO dev. board with this Microcontroller. I don't want to use the Cube generator. I want to use the stdperiph driver without ha...

ilias by Associate II
  • 5097 Views
  • 6 replies
  • 0 kudos

PWM with Dithering (AN4507) firmware--where?

Posted on September 17, 2014 at 01:59Hello, all.  I am looking for the firmware examples for AN4507 (PWM resolution enhancement through dithering technique for STM32 advanced-configuration, general-purpose and lite timers). The document mentions STS...

stm32f7 video compression

Posted on September 07, 2015 at 11:40Good day,I have tried to use new discovery f7 board with camera.It works fine, for now I am writing uncompressed video to avi file in microsd card.I wanted to ask which codec to use for video compression, like xv...

hitsumen by Associate II
  • 802 Views
  • 0 replies
  • 0 kudos

Crystal LSE startup problem on STM32F103RD

Posted on September 03, 2015 at 09:23 Hello, We're using an STM32F103RD for one of our product and on which an extrenal crystal (768Khz) is connected on OSC32 In and ON (LSE). My problem is that this crystal only start to oscilla...

Nucleo F411: 3 synchronized PWM with different number of pulses

Posted on August 14, 2015 at 15:22Hello,is there a way to make 3 synchronous PWM outputs of 100kHzthat each of output would generate particular amount of pulses and then stop?I saw:  https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm3...

algis by Associate II
  • 3375 Views
  • 8 replies
  • 0 kudos

STM32F107VCT6 - programming via USART1

Posted on September 04, 2015 at 18:20Dears,I've got Core107V board from Waveshare with STM32F107VCT6 (rev.Z) and I want to flash my program using USART1.I've plugged FTDI converter the board according to the information in datasheet.3.3V => 3.3V on ...

rybaryba by Associate II
  • 1776 Views
  • 4 replies
  • 0 kudos

SPI Peripheral data bit size on STM32F072

Posted on June 22, 2015 at 22:59Hi.So I'm having a peculiar problem with the SPI on the STM32F072.I'm trying to configure SPI1 and it seems to work, but with one cave-eat. I can't seem to configure the bit size (SCLK) down to 8b from 16b. I've been ...

0690X00000605HfQAI.png
bjerman by Associate II
  • 2709 Views
  • 5 replies
  • 0 kudos

[solved]stm32f0 rtc pls help

Posted on August 21, 2015 at 17:08 I downloaded application note write code.my device(stm32f0discovery,stm32f051r8t6).the weird thing with cube generated code it doesnt work either.In addition if I put breakpoint on while loop when I look rtc I s...

aaslan by Associate II
  • 1968 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.