STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC AWD INterrupt not triggering

Posted on September 19, 2015 at 19:25 Hi Every one, I am trying to establish AWD Interrupt when the voltage value exceedsADC_ITConfig(ADC1, ADC_IT_AWD, ENABLE); I dont know for what reason Is my interrupt not triggering, I try to turn on LED if ...

puneethj by Associate II
  • 1385 Views
  • 2 replies
  • 0 kudos

Merging sample Firmware, CubeMX version

Posted on September 18, 2015 at 20:41In the old days on the B-eval F1 board, I would pick out some sample FW projects and hand merge them into one bigger working monolith - and then use that as a starting point.......but now we have cubeMX and I'm l...

estersci2 by Associate III
  • 1095 Views
  • 1 replies
  • 1 kudos

DWT as a 32-bit timer?

Posted on September 19, 2015 at 14:51A question for Clive (or anyone else who knows that).If I understand right, DWT is a 32-bit timer with CPU frequency. If MCU doesn't have 32-bit timer or has only one and I need let say two of them, is it OK (all...

matic by Associate III
  • 3320 Views
  • 3 replies
  • 0 kudos

MIPS Calculation

Posted on September 18, 2015 at 19:02Hi.I have developed a project and now i have been asked about Mips that i used from ARM device(I'm using STM32F4xx).I'm using IAR Compiler. I will be thankful if every body guide me.thank you. #mips

STM32303e-eval source code

Posted on September 19, 2015 at 00:47The firmware that came loaded on the STM32303e-eval board does not appear to be the same as the source code that the documentation links to: http://www.st.com/web/en/catalog/tools/PF258224♯I'm using Atollic and t...

dhedin by Associate
  • 1010 Views
  • 0 replies
  • 0 kudos

Porting STM32F4 SPI -> STM32F7 SPI

Posted on September 17, 2015 at 23:20Good day,  I tried to port STM32F4discovery SPI to STM32F7discovery SPI, without any luck.  Can you please help me with that.  Here is my code.  I want to port this function:uint8_t SPI_SEND_DATA(uint8_t data){  ...

hitsumen by Associate II
  • 2120 Views
  • 5 replies
  • 0 kudos

HAL bug hanging when an error occurs

Posted on September 18, 2015 at 19:36Hi, There is a bug in function SD_CmdResp1Error. Whe using FatFS with SDIO, when mount fails but the f_open is called, the system hangs in following function: static HAL_SD_ErrorTypedef SD_CmdResp1Error(SD_Handle...

Osto by Senior
  • 606 Views
  • 0 replies
  • 0 kudos

STM32F042 CAN problems

Posted on September 18, 2015 at 09:58 Hi, I have difficulties to enable CAN module on STM32F I did not face problems with CAN module on STM32F1, STM32F2, STM32F4, but now I'm stuck on STM32F0. 1. First, I'm confused from the peripheral l...

search does not work

Posted on September 01, 2015 at 15:00for several days now a search leads to this message:The search request was unable to connect to the Search Service.

Cannot search STM communities

Posted on September 10, 2015 at 16:52Is this a browser problem?  I get the following message using Chrome when I try to do a search:The search request was unable to connect to the Search Service.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.