2015-09-18 10:36 AM
Hi,
There is a bug in function SD_CmdResp1Error. Whe using FatFS with SDIO, when mount fails but the f_open is called, the system hangs in following function: static HAL_SD_ErrorTypedef SD_CmdResp1Error(SD_HandleTypeDef *hsd, uint8_t SD_CMD) { HAL_SD_ErrorTypedef errorstate = SD_OK; uint32_t response_r1; while(!__HAL_SD_SDIO_GET_FLAG(hsd, SDIO_FLAG_CCRCFAIL | SDIO_FLAG_CMDREND | SDIO_FLAG_CTIMEOUT)) { } if(__HAL_SD_SDIO_GET_FLAG(hsd, SDIO_FLAG_CTIMEOUT)) ....................... The system hangs in while loop and come never out of it (only after reset). I dont know the exact reason but this HAL-Code seems to be forgotten to write. OstoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.